New community facilities in the shadow of London’s fire-ravaged Grenfell Tower have opened with energy efficient air conditioning and hot water systems donated by Daikin UK in partnership with installer All Seasons Group Services. The systems serve the newly built St Mark’s Road premises of the Dale Youth Boxing Club and the North Kensington Community Centre – both featured in BBC One’s DIY SOS Grenfell Special. The two-part TV programme was broadcast in September 2018.
Daikin partners with All Seasons Group Services to donate HVAC system installation for boxing club destroyed in Grenfell Tower fire
For both companies, the project brought challenges of delivery, installation and commissioning while working around an army of other volunteer tradespeople – and the TV production team – on a busy 750m2 site underneath the A40 Westway, a short distance from Grenfell Tower. Loughton-based All Seasons Group Services is a Daikin D1+ Partner, and has been installing Daikin systems since 2001.
“Originally we were asked to design an air conditioning installation – but were not told anything about the overall project. When we were told it was to help the community so deeply affected by the Grenfell fire, we had no hesitation in arranging to donate the systems and asking All Seasons to undertake the installation, also as a donation. “As a result, both the club and the community centre will benefit from tapping into a free source of renewable energy and cost-effectively converting it into usable heat."
- Martin Krutz - Daikin UK Managing Director
Daikin high-capacity mini-VRV heat pump
The new gym has a Daikin high-capacity mini-VRV heat pump, serving four RoundFlow cassettes to provide space heating or cooling, as required. It further serves club founder Mick Delaney’s upstairs office, where a wall mounted unit has been installed. The community centre also has a Daikin high-capacity mini-VRV heat pump, which serves nine floor-standing chassis units that are concealed by architectural detailing. Founded some 60 years ago, the boxing club was based in Grenfell Tower from 1999 until the tragic fire in June 2017. The gym had relocated to refurbished premises on a different floor at the base of the building just weeks before the fire. For more than a year after that it operated from a disused multi-storey car park.