Skip to main content

City Centre Hotel

London, UK

Replacing outdoor units for air conditioning systems at central city hotels typically leads to two key challenges: securing road closures and avoiding disruption of hotel operations – or guest comfort.

When two large rooftop chillers at a six-storey hotel in the Blackfriars area had to be replaced, these challenges were very real for installer Chris Henderson, Key Account Manager of Edenbridge-based Nationwide Air Conditioning.

"A new system was needed quickly—but we had to maintain cooling capability throughout"

- Chris Henderson, Key Account Manager of Edenbridge-based Nationwide Air Conditioning

Using two Daikin 560kW air-cooled screw chillers to replace the old units, Nationwide completed the project with the most demanding parts – hoisting units to and from the plant area at the rear of the building – squeezed into two week-ends. And, despite high occupancy levels in at hotel, the work was largely unseen and unheard.

"We designed a solution based on the Daikin units, which offer an attractive combination of price and efficiency. Both chillers’ water connections were handed in the factory to suit the existing on site pipework to reduce major pipework modification and assist with changeover," says Chris Henderson.

“On the first weekend we removed the worse of the two old units, leaving the other system as the sole source of cooling. We then brought in the first of the new 4,785Kg Daikin chillers. Over the following week, the new chiller was connected and commissioned. The second weekend saw the removal of the remaining old unit and installation of the other Daikin chiller."

“The new chillers have much higher specification than the old units. There is ample capacity, so normal demand on each chiller is economically low and one chiller can comfortably handle a peak load, even if the other system is out of action – during maintenance, for example.”

Learn more

Our other cases

  • 60 Grays Inn Road

    Flexible heat recovery solution for Work space tenants
  • A high efficiency solution for a residential building

    This residential project was executed in the context of the renovation of a residential building, which had energy efficiency as a main aspect.
  • ACTION

    As a discount retailer, cost has been a major factor in the choice of HVAC systems for Action, who sought an HVAC supplier that could also give HVAC design and support and offer local coordination in each expansion country.
  • Action reclaimed refrigerant allocation

    Action intensifies its partnership with Daikin for this new ground breaking project: reclaiming refrigerant from its refurbished stores and reusing it.
  • Albany House

    It’s ‘new Daikin for old’ as council upgrades offices for tenants
  • Architectural heritage site

  • Ascent Farnborough

    ‘Easy’ ducted solution ensures comfort in new tenant’s huddle zones
  • Ashcraig, Scotland

    Heat pump delivers a steady temperature and baby sleeps better
  • Astor House

    Newbury office building pioneers Daikin R32 chillers
  • British Airways i360

    Vital role for Daikin VRV IV at high-flying new tourist attraction
  • Bang and Olufsen

    Silence is cool for audio retailer's air conditioning selection
  • Beaumont Court

  • Bennachie Hills, Aberdeen

  • Bennett Homes, East Anglia

    Award-winning East Anglian housebuilder Bennett Homes has a clear specification for comfort and efficiency in future newbuild properties – Daikin Altherma heat pumps for heating and hot water, wherever possible.
  • Best Western Moores Hotel, Guernsey

    Guernsey hotel’s air conditioning changes colour to match new decor
  • Blakes Farm, West Sussex

    Daikin gas boiler gives kitchen sink ‘life-changing’ hot water
  • BrewDog Hotel

    Daikin’s in the DogHouse – air conditioning ‘carbon negative’ hotel
  • Carlton Club, Portsmouth

    Daikin R32 systems bring year-round comfort for Carlton Club members
  • Cawsand Bay

    Efficient, eco-friendly heating for luxury Cornish beach homes
  • Cha No Ma

    Air purification with advanced streamer technology complements Daikin’s environmentally friendly R-32 systems to create a comfortable and healthy café experience.
  • Chester Hotel, Aberdeen

    Illuminating solution for air conditioning in five star hotel and conference centre
  • A Chiller Solution For A Complex Of Office Buildings

    Daikin has recently provided its chiller solutions for an office building project in Krakow, Poland.
  • chillers with R-32 refrigerant at Heinzinger electronic

    An air-cooled chiller from Daikin with a scroll compressor and an output of 200 kW is used, which for the first time works with the climate-friendly refrigerant R-32 and is characterised by optimal operating behaviour and high energy efficiency.
  • Citadines Hotel, Barbican

    Apart’hotel picks heat recovery for greater comfort and efficiency
  • Citadines Hotel

    New chiller takes the heat off London apartment hotel guests
  • City Centre Hotel

    Chiller change boosts comfort at central London hotel.
  • Classic Cottage, Cornwall

    High temperature heat pump gives classic cottage a 21st century boost
  • Providing a complete HVAC system for a food processing plant

    Daikin recently supplied a complete HVAC system to meet the cooling needs of a food processing plant in Hungary. The end user operates in the supplements business, producing plant-based supplements including vegan proteins.
  • Conversion of an old R-22 system

    Conversion of an old R-22 system to a VRV 5 S-series with R32 refrigerant
  • Cooling and heating for small residential buildings

    Daikin BLUEVOLUTION heat pumps have been installed in a number of residential projects, including a recent project in Porto, Portugal.
  • cooling concept for the Engelbert Strauss CI Factory

    Given the gigantic dimensions of the Engelbert Strauss CI Factory, it’s important to keep a cool head.
  • Coral Hatfield

    Coral first past the post with Daikin’s ‘invisible’ air conditioning
  • Council Offices, UK Local Authority

    Heat recovery helps cut costs at ‘smarter’ council offices.
  • Courtyard Hotel Paris

    The Courtyard conversion marks a successful collaboration between forward- looking urban regeneration and Daikin’s flexible, future-proof VRV heat recovery technology.
  • Coventry University Technology Park

    ‘Techno’ park gets an air conditioning technology makeover
  • CP Sierra Engineering

    R32 technology brings cost-saving comfort to engineering staff
  • Croakers Hatch

    Mega Watts house is high-tech temple of heat pump technology
  • Crowne Plaza, Basingstoke

    Hotel’s happy as heat recovery air conditioning heads off heatwave.
  • customised air conditioning for shopping centre

    Read about a complete solution by Daikin for the Intro Bergheim shopping centre with 22 retail units in the centre of Bergheim near Cologne
  • Daikin Emura, design solution for residential living

    Let’s take a look around this apartment in the centre of Milan, Italy’s renowned design and fashion capital. Did you notice the new white Daikin Emura on the wall? It’s an elegant design that beautifully blends into the interior.
  • Dale Amateur Boxing Club

    Daikin partners with All Seasons Group Services to donate HVAC system installation for boxing club destroyed in Grenfell Tower fire
  • David Lloyd Club, Norwich

  • David Lloyd Beaconsfield

    Smart looking gym switches to the stylish Madoka controller
  • Dean Clough Mill

    VRV Heat Recovery helps reshape historic mill into comfortable offices
  • Denstone Hall Farm

    VRV IV system a great comfort for people and perishables.
  • Desco showroom

    Daikin’s ‘plug and play’ rooftop system offers sustainable year-round climate control solution for customer showroom
  • Dickleburgh Stores

    ZEAS updates refrigeration technology for rural convenience store
  • Engineer’s quest for efficiency and comfort proves a real game-changer

  • Energy efficiency

    Daikin has recently provided HFO screw inverter chiller technology solution to major pharmaceutical company for one the manufacturing sites in Wien, Austria.
  • Extension of the L∞P programme by Daikin to chillers

    Daikin Applied Europe has recently extended the L∞P programme by Daikin to chillers. Thereby, Daikin is the only manufacturer actively promoting and supplying units with reclaimed refrigerants, for a wide range of products, from screw and scroll compressor units to centrifugal compressor machines.
  • Fix 8 Group, Manchester

  • Grand Central Hotel Northern Ireland

    Grand, centralised air conditioning system for new Belfast hotel
  • Grand Hotel York

    A grand air conditioning solution for extension of York’s top hotel
  • Great Eastern Street Hotel

    Shoreditch boutique hotel trials Precision Piping Method for ease of installation on site
  • Halcyon Medical

    Strip and rebuild service solves new clinic’s rooftop heat recovery need
  • Handelsbanken Halifax Branch

    VRV spins a comfortable workplace for bankers in converted mill
  • Hafod Caves

    Renewable energy solves key heating issues in Welsh valley cottage
  • High energy efficiency for comfort cooling in Middle East conditions

    Daikin has recently supplied chillers to provide comfort cooling in Middle East conditions in a project involving a four stars hotel in the city of Riyadh, in Saudi Arabia.
  • Historic Cornish Cottage

    Cornish mill conversion upgrades to latest air source heat pump
  • Hock Ridge Farm

  • Holiday Inn Express

    Auto-cleaning duct beats hotel dust, boosting comfort and economy
  • Homefield Grange Spa

    Heat pumps provide efficient, quiet comfort in a spa extension.
  • Residential property with home office

    Building a new residence with an all-round climate control solution
  • Hotel St. Annen

    Located in a quiet residential street in central Hamburg, the Hotel St Annen creates a warm and welcoming ambience for visitors in modern surroundings.
  • Hoteles Santos • Las Arenas

    The Daikin VRV replacement system was the perfect solution for a system upgrade to reduce the energy consumption while keeping the hotel business uninterrupted.
  • Hotel Refurb Central London

    Chiller change boosts comfort at Central London hotel
  • Hyde Park Gardens

    ‘Unseen’ mini-VRV solution beats urban planning constraints
  • Is R-32 really losing relevance in the refrigerant game?

    Daikin’s BLUEVOLUTION heat pumps are being integrated with drain-back solar system kits in small sized residential projects to use solar energy for hot sanitary water production.
  • Japan House, Kensington

    Daikin heat recovery ‘on show’ at Japanese cultural centre in London
  • JBC

    In its ongoing search to optimise running costs, JBC conducted a site trial with Daikin designed to evaluate the gains generated by Variable Refrigerant Temperature (VRT) technology.
  • K-Way

    Daikin’s ‘greener’ solution for Covent Garden retail premises
  • Kew Road

    Water-cooled VRV perfect solution for Richmond office refurbishment
  • Kings Park Village

    Some like it hot – especially when a heat pump cuts energy bills
  • L1 DOT Complex Poland

    Daikin teams up with building designers to maximise BREEAM* rating with its commercial heat pumps
  • Lansdowne Road

    Cambridge family graduates to a cool new Daikin R32 solution
  • Leon restaurant

    Synecore installs the first of Daikin’s VRV IV i-Series integrated plant
  • London Bank

    Bank’s chilling ‘green’ solution accounts for big cost savings
  • Lush Store, Edinburgh

    ‘Invisible’ air conditioning a Lush comfort solution for Edinburgh
  • Making hospitals more efficient

    Daikin has recently taken part in an important project involving hospitals in Istanbul, Turkey. It is a government project, aiming at making hospitals more energy efficient through the replacement of chillers and other components of the HVAC system that provide these buildings with cooling or heating.
  • Meeting a hospital’s cooling needs and keeping power input low

    Daikin has recently provided chillers for one of the biggest private hospitals in Qatar. The hospital has world-renowned international affiliations and the mission to provide optimal patient care by utilizing unparalleled and advanced services.
  • Merlin Properties

    As part of a business center in Madrid, this office complex was upgraded to a more efficient solution, while keeping investment costs under control.
  • Merlin Housing

    Social Housing Refurb - Social tenants anticipate ‘exceptional’ savings with heat pumps
  • Montcalm Hotel

    ‘M’ picks Daikin VRV for five-star hotel comfort and efficiency
  • Naturkost Brinkman

    Organic specialist retailer Naturkost Brinkman uses Daikin retail refrigeration to deliver improved energy efficiency and in-store comfort.
  • New office building for hotel outfitter TKS in Borken

    Daikin provides heating, cooling and ventilation for hotel outfitter TKS in Borken
  • Office Premises in Malvern

    Techno’ firm future-proofs new premises with Daikin R32 systems
  • Office refurbishment in Madrid, Spain

    Daikin’s VRV 5 S-Series provided the ideal solution for a refurbishment project of a semi-detached villa in Madrid
  • Oxford Brookes University

    Low-GWP technology helps busy university servers keep cool
  • Perial Asset Management

  • Pomme d'Or Hotel

    Hotel’s golden opportunity to trim costs with auto cleaning ducts
  • Hotel Santos Porta Fira

    The Santos Group, the organisation in charge of building Porta Fira, selected Daikin as a trusted partner to deliver a unique, reliable and energy-efficient climate control system for the building.
  • Portcullis House

    Daikin VRV IV delivers a healthy extra benefit – more lettable space
  • Prezzemolo & Vitale - Palermo

    For the new Prezzemolo & Vitale store in the historical centre of Palermo, a system was installed consisting of Daikin Zeas and VRV units.
  • Providing cooling & heating for small residential buildings

    Daikin’s BLUEVOLUTION heat pumps are being integrated with drain-back solar system kits in small sized residential projects to use solar energy for hot sanitary water production.
  • Providing cooling for an industrial manufacturer of automotive components

    Daikin recently supplied an air-cooled screw inverter chiller unit from the TZ Series to meet the cooling needs of an industrial plant near Lisbon, Portugal. The facility manufactures brakes and other components for the automotive industry.
  • Refrigerant removal Bristol Waters

    'A' team cuts time and costs on refrigerant recovery mission
  • Royal Marsden

    Hospital saves a cool £53k a year after air conditioning upgrade
  • Samrya 44

    With 44 floors of elegantly-designed luxury suites, Samrya 44 adheres only to the highest standards in construction and HVAC.
  • Smith and Wollensky

    Daikin help high-end steakhouse serve full flavour - and comfort
  • Sound enclosure case study in Flassy

    The acoustic effectiveness of Daikin’s new Sound Enclosure for its Sky Air and VRV 5 outdoor units has been validated by field trials undertaken at a residential installation in Burgundy, France, showing significant sound reductions equal to and even exceeding factory test room values.
  • St George's Kew

    Daikin’s on ‘Kew’ for comfort cooling at riverside apartments
  • Bennett Homes, East Anglia

    Award-winning East Anglian housebuilder Bennett Homes has a clear specification for comfort and efficiency in future newbuild properties – Daikin Altherma heat pumps for heating and hot water, wherever possible.
  • Taper Studios London

    Taper’s business services are out of mind for residents upstairs
  • The Bloomsbury Hotel

    The VRVIII Heat Recovery System from Daikin was selected for its supremely low energy consumption and ability to off er massive savings in comparison with similar systems
  • The Jungle

    Air conditioning solution tames a ‘steamy’ Jungle – all year round
  • The Boston Mayflower

    Space-saving heating boost for Boston bungalow
  • The Croke Family, Guildford Case Study

    ‘Alexa, please switch the boiler on’
  • The Salthouse Hotel, Northern Ireland

    Nature-powered heat pumps play key role at pioneering eco-hotel.
  • The Warrington Family, Swinton

    New Daikin gas boiler set to ‘condense’ family’s heating costs
  • Thirteen Group

  • Training Centre Belgium

    Daikin sought a future-proof low energy HVAC solution for its new Training Centre located in Ghent.
  • Uttoxeter Racecourse

    Uttoxeter Racecourse backs a cool winner with Daikin R32 splits
  • Velocity office building

    Sustainability is at the forefront of Velocity's design. Each element of the design has been carefully considered to ensure an EPC rating of "B" and an "Excellent" BREEAM rating has been achieved.
  • VRV heat pump contributes to low carbon footprint

    The new Arteparc commercial complex situated in the Inovallee techpark in Meylan, Grenoble demonstrates how developers and equipment manufacturers are working together to deliver new lowcarbon buildings that align with the highest standards of sustainable development.​
  • Warm pool water through heat recovery

    State-of-the-art Daikin integrated heat recovery technology saves a significant amount of energy and heats the water in the hotel's pool.
  • Weir House, Bristol

    Weir House conversion raises the flag for renewables in Bristol
  • Wensum Place, Bromley

    Homeowner hoping for a hot summer to try out new Daikin R32 system
  • West Thames College

    Heatwave prompts college switch to Daikin heat recovery system
  • What to consider when choosing a heat pump for a residential building

    What to consider when choosing a heat pump for a residential building
  • Wilton Row Project

    Compact single fan VRV IV S-series an ‘unseen’ solution in Belgravia
  • Yorkshire Hotel

    Hotel’s chilled water fan coil upgrade an all-round winner
  • Zome

    The hubs from ZOME are modern and agile spaces to offer a personalised experience to customers.
  • 40 Clarendon Road

  • Electricity North West

  • Quayside Lodge

    Daikin’s low carbon, heating, cooling and heat recovery solution for a prestigious London Conservation Area development

Get support, guides & logins

Contact Us

Get information & support

Contact a Daikin installer

Contact Us

Get installer information & support

Contact Us

Get information, CPD and certifications

Contact a Daikin installer

Contact Us