Skip to main content

Hoteles Santos • Las Arenas

Valencia, Spain

Lowering operation costs while staying operational

The existing HVAC-R system was installed in 2007. After 13 years, a system update was preferred to enhance efficiency. The latest technological advancements of new Daikin systems ensure a future-proof and energy-saving operation while keeping a top level comfort. Even the existing indoor units and piping could be reused, so there was no need to close the hotel for a renovation.

With this system update an efficiency increase of 30 % was achieved right from the start. Compared with a complete new installation this was reached with a much lower investment. The fast and gradual installation reduced business disturbances to a minimum and allowed to keep the hotel open during the whole installation process.

Solution at a glance

  • 88 outdoor units
  • 458 indoor units
  • Central control with Intelligent touch Manager
  • Installation and maintenance monitoring with Daikin Cloud Service

Learn more

Our other cases

  • Quayside Lodge

    Daikin’s low carbon, heating, cooling and heat recovery solution for a prestigious London Conservation Area development
  • VRV heat pump contributes to low carbon footprint

    The new Arteparc commercial complex situated in the Inovallee techpark in Meylan, Grenoble demonstrates how developers and equipment manufacturers are working together to deliver new lowcarbon buildings that align with the highest standards of sustainable development.​
  • Providing a complete HVAC system for a food processing plant

    Daikin recently supplied a complete HVAC system to meet the cooling needs of a food processing plant in Hungary. The end user operates in the supplements business, producing plant-based supplements including vegan proteins.
  • Extension of the L∞P programme by Daikin to chillers

    Daikin Applied Europe has recently extended the L∞P programme by Daikin to chillers. Thereby, Daikin is the only manufacturer actively promoting and supplying units with reclaimed refrigerants, for a wide range of products, from screw and scroll compressor units to centrifugal compressor machines.
  • Bennett Homes, East Anglia

    Award-winning East Anglian housebuilder Bennett Homes has a clear specification for comfort and efficiency in future newbuild properties – Daikin Altherma heat pumps for heating and hot water, wherever possible.
  • Is R-32 really losing relevance in the refrigerant game?

    Daikin’s BLUEVOLUTION heat pumps are being integrated with drain-back solar system kits in small sized residential projects to use solar energy for hot sanitary water production.
  • Providing cooling & heating for small residential buildings

    Daikin’s BLUEVOLUTION heat pumps are being integrated with drain-back solar system kits in small sized residential projects to use solar energy for hot sanitary water production.

Get support, guides & logins

Contact Us

Get information & support

Contact a Daikin installer

Contact Us

Get installer information & support

Contact Us

Get information, CPD and certifications

Contact a Daikin installer

Contact Us