Skip to main content

Cooling and heating for small residential buildings

Daikin BLUEVOLUTION heat pumps have been installed in a number of residential projects, including a recent project in Porto, Portugal.

Products Installed

2x EWYT-CZ

Total cooling capacity: 21 kW

Total heating capacity: 21 kW

 

About the project

The customer wanted a solution that could provide cooling or heating based on seasonal needs, as well as hot sanitary water. The solution also needed to be reliable and offer high energy efficiency and low running costs.

 

More about the project, the solution and the product

The new R-32 Small Inverter Chiller has proved itself to be a valuable solution in a wide range of situations, ranging from big stadiums to relatively small houses.

For this project, Daikin supplied two heating units that easily met the required capacity needs (21 kW) and provided the highest energy efficiency in the market for its product segment.

The R-32 Small Inverter Chiller was installed as part of a system to provide cooling or heating (based on the season) to indoor fan coils, as well as hot sanitary water. Thanks to its modern design and advanced technology that optimises full inverter units, the unit met all the project’s requirements, provided outstanding efficiency, and delivered excellent performance with a low GWP refrigerant such as R-32.

Read more here about the new Small Inverter Chiller

 

Daikin’s extensive experience in developing R-32 technology ensures the unit’s reliability.

In 2018, Daikin was an early innovator and made history by introducing the first R-32 refrigerant chillers, followed by free-cooling scroll units the same year, and the R-32 Heat Pump in 2020.

Today, Daikin has the highest number of R-32 installations in the world. This is a testimony to the experience, knowledge, quality, and reliability of its R-32 products.

Read more here about Daikin being pioneers in R-32 technology development

 

Are you interested in learning more about the new Daikin R-32 Small Inverter Chiller? Contact us via the form below.

Related articles