Daikin, world’s first company introducing a new generation of air cooled scroll chiller series with refrigerant R-32.
Daikin is continuously leading in chiller technology, striving again for innovation. With the new generation of chillers and heat pumps with R-32, Daikin has extended the Bluevolution range to larger capacities, allowing commercial applications as well to benefit from from the use of R-32 refrigerant.
Why has Daikin introduced R-32 models?
The Global Warming Potential (GWP) of R-32 is only 675. Only one third compared to a commonly used refrigerant such as R-410A. Thanks to the lower flammability classification (R-32 falls into the class A2L category in ISO817), it can be safely used in many applications - chilled water systems included. Then, as a single component refrigerant, it can be easily recycled and reused - another environmental plus in its favour.
Why choose R-32 refrigerant
As a matter of fact, R-32 refrigerant is considered the most balanced refrigerant in terms of Environmental Impact, Energy Efficiency, Safety and Cost-Effectiveness for AC and Heat Pump equipment.
Let’s start analyzing how R-32 responds to the main aspects to consider when choosing refrigerant: affordability, environmental friendliness and safety.
An insight on Daikin’s refrigerant policy and response to new needs
Refrigerants are more than ever necessary since the cooling and heating needs of our world are growing. While refrigerant solutions of the past may have had consequences on today’s environment, it is important to find future-proof solutions to current challenges now. That is Daikin’s main goal. Contributing to mitigating refrigerants environmental impact with a comprehensive approach throughout refrigerant and equipment lifecycle.
When choosing a refrigerant, the main aspects to consider are usually safety, affordability, and environmental friendliness. It is a matter of balance between these different aspects and factors. Of course, choices might differ depending on the application, as a single perfect choice for any application simply doesn’t exist. But the recent changes introduced by new international regulations have led to new developments in the world of refrigerants, which has been moving towards lower GWP refrigerants in the recent years.
Daikin, as company who has a unique expertise coming from manufacturing and producing both refrigerants and equipment, has identified R-32 refrigerant as the most balanced refrigerant in terms of Environmental Impact, Energy Efficiency, Safety (R-32 is classified as a A2L - low flammability) and Cost-Effectiveness for AC and Heat Pump equipment. That is why Daikin believes in R-32.
EWAT-B
EWYT-B
EWAA-DA
EWAT-CZ
EWYA-DA
EWYT-CZ
The Bluevolution range is about to be extended with the introduction of a new Series completing this product family by Daikin for the Commercial Air Conditioning segment.
The Bluevolution range is made of modern and advanced technologies featuring R-32 refrigerant. These products aim to significantly reduce the environmental impact of Air Conditioning technologies for the commercial sector. All this, without affecting the performance of the units and their ability to produce the required level of comfort. Get in touch to know more!
Refrigerants are more than ever necessary, since the cooling and heating needs of our world are growing. While refrigerant solutions of the past may have had consequences on today’s environment, it is important to find future-proof solutions to current challenges now. That is Daikin’s main goal. Contributing to mitigating refrigerants environmental impact with a comprehensive approach throughout refrigerant and equipment lifecycle.
Daikin, as company who has a unique expertise coming from manufacturing and producing both refrigerants and equipment, has identified R-32 refrigerant as the most balanced refrigerant in terms of Environmental Impact, Energy Efficiency, Safety (R-32 is classified as a A2L – low flammability) and Cost-Effectiveness for AC and Heat Pump equipment. That is why Daikin believes in R-32 and keeps developing cutting-edge technologies based on this refrigerant.
Stay tuned for more information on the upcoming product launch!