The right temperature helps you sleep better
Restful sleep requires not only a good bed, but also the right environment: quietness, darkness and a low temperature. The optimal temperature depends on your personal requirements. And even this temperature adjusts to outside temperatures. By keeping the temperature at a low level, higher oxygen levels are kept, which are essential for the regeneration of your body.
Window open or closed at night?
Nothing’s more pleasant than sleeping with the window open, right? But this is often not helpful, especially in cities: heated streets, light and noise prevent a restful sleep. This is where air conditioning comes in: the perfect feel-good temperature with the push of a button! Quiet and comfortable.
High temperatures mess with your brain
Temperatures above 26 °C reduce concentration and performance by about 30 %. Your brain needs a lot of oxygen. So, keeping the temperature below 26°C will definitely make you feel better and perform effectively.
Your body’s built-in cooling system: sweat
In addition, your body automatically starts a protective programme at high temperatures. You start to feel tired to prevent dangerous overheating through physical activity. If the outside temperature is around 30 °C, the body activates its built-in cooling function: sweat. The cooling effect of sweating occurs through evaporation on your skin.
Daikin helps to keep your brain active
The higher the humidity on hot days, the less sweating works effectively. Your energy goes into sweating and is missed by the brain. Daikin air conditioners don't just cool. They also have a dehumidification function, which should not be underestimated here in particular.
Summertime means allergies time
Many of us suffer from pollen allergies in summer. And exposure to other particles in the air (allergens, pathogens, fine dust, irritating odours) is generally higher in summer than in winter.
The positive effects of pure seaside air at home
Especially at the seaside, these pollutants are noticeably lower. What is the cause? For one thing, fewer polluting particles are released. For another, the large surface area of water offers a high purification function.
But even in your own home you are not defencelessly exposed to these pollutants: Daikin air purifiers as well as Daikin air conditioners have several highly efficient filter technologies to retain and inactivate such particles.
Don’t wait until you’re too late
Summer is coming. Get ready to protect your home against the heat waves to come. If you wait for the first sweaty nights, it might be hard to find a trained installer to advise you on Daikin air conditioning systems.