Skip to main content

Suppresses not only the viruses that cause colds and flu, but also the Respiratory Syncytial Virus (RSV)

Influenza type A virus with strong symptoms and infectivity

There are three types of the influenza virus: type A, type B, and type C. Among them, type A has particularly strong symptoms such as high fever. It is called a threatening influenza virus because it is extremely infectious and spreads quickly.

* The results are obtained from demonstration of solely the Daikin Streamer discharge device in an experimental condition.

Demonstration of the suppression effect against influenza virus (type A, H1N1)

Testing organization

Kitasato Research Center for Environmental Science

Test method

By irradiating the influenza virus with Streamer and inoculating the cultured cells, we observed the residual state of the virus by the difference in the Streamer irradiation time.

Streamer - surpression effect against influenza virus type A H1N1

As a result of the experiment, it was confirmed that 99.9% of influenza virus (type A, H1N1) was decomposed within 1 hour of Streamer irradiation.

* The results are obtained from demonstration of solely the Daikin Streamer discharge device in an experimental condition.

Demonstration of the suppression effect against influenza virus (type A, H3N2)

Testing organization

Shanghai City Center for Disease Control and Prevention, etc.

Test method

By irradiating the influenza virus with Streamer and inoculating the cultured cells, we observed the residual state of the virus by the difference in the Streamer irradiation time.

Streamer - surpression effect against influenza virus type A H3N2

As a result of the experiment, it was confirmed that 99.0% of influenza virus (type A, H3N2) was decomposed within 4 hours of Streamer irradiation.

* The results are obtained from demonstration of solely the Daikin Streamer discharge device in an experimental condition.

Demonstration of the suppression effect against respiratory syncytium virus (RS virus)

Testing organization

Wakayama Medical University

Test method

By irradiating the RS virus with the Streamer and inoculating the cultured cells, we observed the residual state of the virus over the Streamer irradiation time.

Streamer - surpression effect against respiratory syncytium virus (RS virus)

As a result of the experiment, it was confirmed that 99.0% of RS virus was decomposed within 8 hours of Streamer irradiation.

* The results are obtained from demonstration of solely the Daikin Streamer discharge device in an experimental condition.