Skip to main content

Suppresses various viruses that cause summer colds and measles

It has been proved that the active elements produced by Streamer technology decompose and neutralize the viruses that cause summer colds and measles by contacting them.

* The results are obtained from demonstration of solely the Daikin streamer discharge device in an experimental condition.

5 viruses that cause summer colds and measles.

Summer colds such as pool fever, herpangina and hand-foot-and-mouth disease are viral infections that prevail in the rainy season and summer, especially among children with a weaker immunity than adults. Four major causes of these summer colds have been identified: adenovirus, enterovirus, echovirus and coxsackie virus. In addition, measles, which spreads from spring to summer, is very infectious because of the measles virus.

Demonstration of the suppression effect against Adenovirus

Main cases of Adenovirus: pool conjunctival fever, etc.

Testing organization

Kitasato Research Center for Environmental Science

Test method

By irradiating the Adenovirus that causes a summer cold with Streamer for 0, 1, 2, 4, 8 hours and inoculating the cultured cells, we observed the residual state of the virus by the difference in the Streamer irradiation time.

Streamer surpression effect against Adenovirus

As a result of the experiment, the 99.9% suppression effect against Adenovirus was confirmed within 4 hours after Streamer irradiation.

* The results are obtained from demonstration of solely the Daikin Streamer discharge device in an experimental condition.

Demonstration of the suppression effect against Coxsackie virus

Main cases of Coxsackie virus: herpangina, etc.

Testing organization

Kitasato Research Center for Environmental Science

Test method

By irradiating the coxsackie virus that causes a summer cold with Streamer for 0, 1, 2, 4, 8 hours and inoculating the cultured cells, we observed the residual state of the virus by the difference in the Streamer irradiation time.

Streamer surpression effect against Coxsackie virus

As a result of the experiment, the 99.9% suppression effect against Coxsackie virus was confirmed within 4 hours after Streamer irradiation.

* The results are obtained from demonstration of solely the Daikin Streamer discharge device in an experimental condition.

Demonstration of the suppression effect against Echovirus

Main cases of Echovirus: hand-foot-and-mouth disease, etc.

Testing organization

Kitasato Research Center for Environmental Science

Test method

By irradiating the echovirus that causes a summer cold, with Streamer for 0, 1, 2, 4, 8 hours and inoculating the cultured cells, we observed the residual state of the virus by the difference in the Streamer irradiation time.

Streamer surpression effect against Echovirus

As a result of the experiment, the 99.9% suppression effect against Echovirus was confirmed within 8 hours after Streamer irradiation.

* The results are obtained from demonstration of solely the Daikin Streamer discharge device in an experimental condition.

Demonstration of the suppression effect against Enterovirus

Main cases of Enterovirus: hand-foot-and-mouth disease, etc.

Testing organization

Kitasato Research Center for Environmental Science

Test method

By irradiating the enterovirus that causes a summer cold with Streamer for 0, 1, 2, 4, 8 hours and inoculating the cultured cells, we observed the residual state of the virus by the difference in the Streamer irradiation time.

Streamer surpression effect against Enterovirus

As a result of the experiment, the 99.9% suppression effect against Enterovirus was confirmed within 8 hours after Streamer irradiation.

* The results are obtained from demonstration of solely the Daikin Streamer discharge device in an experimental condition.

Demonstration of the suppression effect against Measles virus

Main cases of Coxsackie virus: measles, etc.

Testing organization

Kitasato Research Center for Environmental Science

Test method

By irradiating the measles virus that causes a summer cold with Streamer for 0, 1, 2, 4, 8 hours and inoculating the cultured cells, we observed the residual state of the virus by the difference in the Streamer irradiation time.

Streamer surpression effect against Measles

As a result of the experiment, the 99.9% suppression effect against Measles virus was confirmed within 8 hours after Streamer irradiation.

* The results are obtained from demonstration of solely the Daikin Streamer discharge device in an experimental condition.