Skip to main content

Decomposes and suppresses Moraxella bacterium, which causes the laundry's damp odor

It is known that the bacteria causing the laundry's damp odor that occurs when drying clothes in the room are Moraxella bacteria. It was confirmed that the Streamer technology decomposes and suppresses the bacteria that cause this damp odor.

* The results are obtained from demonstration of solely the Daikin Streamer discharge device in an experimental condition.

Demonstration of the suppression against Moraxella bacterium Bacillus (causative agent of the laundry's damp odor)

Testing organization

Japan Food Research Laboratories

Test method

A sample containing 2 ml of the test bacterial solution in a petri dish (φ60 mm) was left to stand in the Streamer generator. The suppression effect was obtained from the results of measuring the number of bacteria after 1, 2, 3, 4, and 6 hours. The Streamer discharge device and test bacteria were provided by Daikin. This was measured 3 times

Survival rate of Moraxella becterium bacills after 2 hours of Streamer irradiaton

As a result of the test, it was confirmed that Moraxella bacterium (causative agent of the laundry's damp odor) was decomposed and suppressed by 99.8% in 2 hours after the Streamer irradiation.

* The results are obtained from demonstration of solely the Daikin Streamer discharge device in an experimental condition.