Skip to main content

Pure air, because we care

With Daikin air purifiers, we promise you air that is cleaner, healthier and fresher.

Effective for cleaning the air and removing:

Viruses

Allergens

Dust particles

Odours

Tested by

IPL

99.98% of coronavirus removed in 2.5 minutes*
As tested by Institut Pasteur de Lille

According to tests performed in the laboratories of the Institut Pasteur de Lille, Daikin’s air purifiers remove more than 99.98% the human coronavirus HCoV-229E in 2.5 minutes*. This virus is of the same family as SARS-CoV-2, the coronavirus behind the COVID-19 pandemic.

The units have also been evaluated as 99.93% effective against the H1N1 virus in 2.5 minutes*.
H1N1 is the virus causing common flu.
This means Daikin’s air purifiers are an additional measure in the fight against respiratory diseases. Our compact plug-and-play purifiers, whose effectiveness is achieved through a combination of the high performance electrostatic HEPA filter, which traps the virus, followed by an intense exposure to Daikin’s patented Flash Streamer technology, which removes the virus, can strongly contribute to reducing the risk of respiratory virus transmission.

Efficient against allergens as recognized by BAF (British Allergy Foundation)

The Allergy UK Seal of Approval reassures that the product is efficient at reducing small particulates which may include allergens, bacteria and viruses.

Approved allergy-friendly quality of this product/service is certified by the European Centre for Allergy Research Foundation​

An independent advisory panel of 15 leading international scientists and technicians has developed the criteria ECARF uses to  evaluate different product groups. They include threshold values and exclusion criteria that make an allergic reaction very unlikely. The criteria are regularly updated to reflect the latest scientific findings. A product receives the Seal when it can be proved through audits or studies that the criteria have been fulfilled. The Daikin Air Purifiers passed these tests and can be considered as allergy-friendly. ​

​

*Daikin device MCK55WVM (commercial name MCK55W), tested by Institut Pasteur de Lille, removes 99.996 % of Human Coronavirus HCoV-229E in 2.5 minutes running time at ‘turbo’ speed in laboratory conditions (air-tight chamber with inner volume 0.47 m3, no air renewal). Human Coronavirus HCoV-229E is different from the virus responsible for COVID-19, SARS-CoV-2, but belongs to the same family of coronaviruses. | Daikin device MC55WVM (commercial names MC55W/VB), tested by Institut Pasteur de Lille, removes 99.98 % of Human Coronavirus HCoV-229E in 2.5 minutes running time at ‘turbo’ speed in laboratory conditions (air-tight chamber with inner volume 1.4 m3, no air renewal). Human Coronavirus HCoV-229E is different from the virus responsible for COVID-19, SARS-CoV-2, but belongs to the same family of coronaviruses. | Daikin device MCK55WVM (commercial name MCK55W), tested by Institut Pasteur de Lille, removes 99.986 % of Influenza A virus subtype H1N1 in 2.5 minutes running time at ‘turbo’ speed in laboratory conditions (air-tight chamber with inner volume 0.47 m3, no air renewal). | Daikin device MC55WVM (commercial names MC55W/VB), tested by Institut Pasteur de Lille, removes 99.93 % of Influenza A virus subtype H1N1 in 2.5 minutes running time at ‘turbo’ speed in laboratory conditions (air-tight chamber with inner volume 0.47 m3, no air renewal).

No maintenance costs for at least 10 years

No need to change the filters in the first 10 years after unit purchase, avoiding additional costs for regular filter changes.

One of the most silent air purifier range on the European market

Our air purifiers are whisper quiet during quiet operation (sound pressure level: 19 dBA), providing you pure air without noticing.

Compact & performing

Small size, but also perfect for very large surfaces.

Breathe in air that is clean and healthy

Daikin air purifiers minimise asthma and allergy symptoms by removing dust particles, pollen and other allergens from your indoor air, helping to keep you healthy by filtering out airborne bacteria and viruses.

The patented Streamer technology in Daikin air purifiers inactivates in more than 2.5 minutes* 99.93% of the common flu virus (H1N1) and 99.98% of the human coronavirus HCoV-229E, which is in the same family as SARS-CoV-2, the coronavirus behind the COVID-19 pandemic.

Humidity is essential for healthy skin

The Ururu streamer technology air purifier offers humidification and purification all in one, to maintain a comfortable humidity level in your home. 

The humidifying air purifier’s slim water tank infuses moisture into the air when it is too dry, to help avoid you getting dry skin or waking up with a scratchy throat.

Indoor air quality is vital for health

According to Allergy UK, people today spend on average 90% of their time indoors. So good indoor air quality is crucial for our health.

Pure indoor air is especially important for vulnerable groups – such as the very young and old, as well as people living with respiratory diseases and allergies. 

Keep your air smelling fresh 

Our air purifiers control odours so that your home smells fresh and clean. Daikin’s Air Purifier is designed to deal with harmful particles, as well as dust, odours, bacteria, pet hairs, moulds, pollen and mites and other allergens, leaving the indoor air clean and healthy.

Remove airborne hazards

At the heart of the Air Purifier is Daikin's Streamer technology, which releases ions into the air and generates active components that attach to the surface of fungi and allergens and decompose hazardous elements. 

The air purifier cleans a space of up to 41m2, taking in air from the front and side of the unit covering a wide area and discharging clean air from the top. The electrostatic filter collects dust effectively without clogging, so it can filter a larger amount of air than typical mesh filters. 

* Source: “Study report on the inactivation effect of plasma ion generator (Daikin Streamer) on SARS-CoV-2” redacted by Shigeru Morikawa, Department of Veterinary Medicine, Microbiology Course, Okayama University of Science

Daikin’s Air Purifiers have gained the Quiet Mark award for delivering the ultimate in acoustic comfort

As the only global award for acoustic design excellence, we’re delighted to confirm that two of our Air Purifier models are now Quiet Mark certified. Daikin’s Air Purifiers (models MCK55WVM and MC55VBFVM) have been thoroughly tested by the Quiet Mark experts and found to be among the quietest products on the market.

Here at Daikin, we recognise that it’s important to help homeowners keep their homes as calm and peaceful as possible. Quiet Mark certification means consumers can easily identify products that won’t add unnecessary noise to their home and help them make informed choices about the appliances they purchase.

bg-image

Institut Pasteur de Lille evaluated the effectiveness of Daikin’s air purifiers against respiratory viruses.

According to tests performed in the laboratories of the Institut Pasteur de Lille, Daikin’s air purifiers eliminate more than 99.98% the human coronavirus HCoV-229E in 2.5 minutes*. This virus is of the same family as SARS-CoV-2, the coronavirus behind the COVID-19 pandemic.

The units have also been evaluated as 99.93% effective against the H1N1 virus in 2.5 minutes*. H1N1 is the virus causing common flu.

This means Daikin’s air purifiers are an additional measure in the fight against respiratory diseases. Our compact plug-and-play purifiers, whose effectiveness is achieved through a combination of the high performance electrostatic HEPA filter, which traps the virus, followed by an intense exposure to Daikin’s patented Flash Streamer technology, which eliminates the virus, can strongly contribute to reducing the risk of respiratory virus transmission.

Explore our Air Purifiers

  • Streamer technology air purifier MC30Y

    The MC30Y Air Purifier filters out airborne particles that van often pose serious health risks. Compact and performing, up to 46 m².

  • Streamer technology air purifier M30YB

    The MC30YB Air Purifier filters out airborne particles that van often pose serious health risks. Compact and performing, up to 46 m².

  • Streamer technology air purifier MC55W

    Our streamer technology filters out airborne particles that can often pose serious health risks.

  • Ururu air purifier with Streamer MCK55W

    The Daikin Ururu air purifier MCK55W purifies and moisturises the air inside your home. Simply fill the 2.7l tank occasionally and it will humidify your room with a maximum rate of 500ml/h.

  • Ururu air purifier with streamer MCK70YV

    The Daikin Ururu air purifier MCK70YV purifies and moisturises the air inside your home. It will humidfy your room with a maximum rate of 650 ml/h, so perfect for an extended surface area.

     

Every breath you take: Daikin Air Purifier review

My Home Farm reviews one of our MC55VB air purifiers.

1 Powerful suction

Takes in air over a wide area from 3 directions.

 

 

Powerful Suction Illustration

2 Effective capturing of pollutants

Efficiently catches dust and pollutants with an electrostatic HEPA filter.

Electrostatic HEPA Filter

3 Decomposition

Uses Daikin's Streamer technology to decompose, by oxidation, harmful substances caught on the filter.*

Streamer

 

* Substances including viruses1, bacteria2, pollen3, mould spores4

Air purifiers de-mystified: How do you know which is right for you

What should you consider before buying an air purifier? What is a HEPA filter? We take you through what you need to know before purchasing an air purifier.

High Performance HEPA filter to catch fine particles of dust

Removes 99% of particles between 0.1μm and 2.5μm in size

The filter collects dust efficiently with electrostatic forces. It is not prone to clogging compared with non-electrostatic HEPA filters which collect particles only by the fineness of the mesh.

 

Electrostatically Charged

Electrostatic HEPA filter

Removes 99,97% of fine particles of 0,3μm Filter fiber itself is charged with static electricity, and collects particles efficiently. Doesn’t clog easily, hence causes low pressure loss.

Therefore, a larger amount of air can pass through the filter.

 

 

 

 

 

 

VS

 

 

 

The filter can purify a larger amount of air!

 

 

 

 

Electrostatically Neutral

Non-electrostatic filter

Because it catches particles relying only on mesh size, it is necessary to make mesh finer, making it easy to be clogged and cause high pressure loss.

Compact, effective and quiet thanks to the new, innovative structure

Air Purifier Structure Illustration

Daikin Air Purifiers are equipped with Streamer technology​

Humidifying Function Illustration

 

Powerful humidification to protect against air dryness and viruses

  • Protects the skin, the throat and the nostrils from dryness. 
  • Protects against viruses by maintaining appropriate humidity of the room. 
  • Maintains comfortable room humidity levels (40 to 60% RH)
  • Streamer eliminates bacteria on the humidifying filter. 

Downloads

Related articles

bg-image

Indoor Air Quality, A Daikin Experience

* Source: Institut Pasteur de Lille test report 2021. Testing laboratory ‘Institut Pasteur de Lille’ France, evaluated the effectiveness of Daikin’s Air Purifiers against respiratory viruses:
- HCoV-229E (of the same family as SARS-CoV-2, the coronavirus causing the COVID-19 pandemic)
- Influenza A virus subtype H1N1 (causing seasonal flu)
Please note: A Daikin Air Purifier is not a substitute for safety measures including smoke and heat detectors and carbon monoxide monitors. A Daikin Air Purifier may not be suitable for extracting odour components emanating from continuous sources – please email airpurifier@daikin.co.uk for more information.

FAQ

The air we breathe at home or indoors is up to 5 times more polluted than the air outside. Thanks to its unique “catch & clean” approach, the Daikin air purifier captures and removes pollutants, reducing indoor pollution and improving the quality of the air in your home, office, shop, etc.​

The Daikin air purifier helps us breathe clean air by essential reduction of viruses, fine dust and allergens. According to tests performed in the laboratories of the Institut Pasteur de Lille, Daikin air purifiers remove at least 99,98% of the human coronavirus HCoV-229E in 2.5 minutes. This virus is of the same family as SARS-CoV-2, the coronavirus behind the COVID-19 pandemic. Daikin air purifiers also helping us to prevent allergies as recognized for example by the reputed British Allergy Foundation. The deodorising filter of Daikin air purifiers successfully captures and absorbs odours wherever it’s needed.

 

The Daikin air purifier is equipped with an advanced filter system that captures viruses, bacteria and allergens meanwhile its patented Streamer technology takes care of removing it and keeping both the indoor air and the air purifier filters clean. The prefilter captures larger particles, trapping them inside. Thanks to its electrostatic capacity, Daikin HEPA filter catches pollutants without clogging the mesh, meaning that it does not need to be replaced for 10 years. The deodorising filter captures and absorbs odours without becoming saturated as happens with traditional activated carbon filters. Finally, the humidifier filter (exclusive to Daikin air purifier model equipped with humidifier) ​​eliminates bacteria in the water tank thanks to the double layer filter with silver ion cartridge. ​

 

Yes, the Daikin air purifier has been tested and certified by the prestigious ECARF institute as an ideal product for people with allergies. Above that the Daikin Air purifier is also recognized as efficient by BAF (British Allergy Foundation). This seal reassures that the product is efficient at reducing small particles which may include allergens, bacteria and viruses.

No, the Daikin Air Purifiers range is recognised as one of the most silent on the market. They are whisper quiet during silent operation mode, providing you with pure air without even noticing. ​

Opposed to other brands, it is not necessary to change a filter of the Daikin Air Purifier in the first 10 years after purchase. Giving you years of clean air with peace of mind.

Thanks to its compact design you can easily pick up and move your Air Purifier to another location. Bad smell in the kitchen? Move your Air Purifier there and let its magic work. Left the window open during Pollen season? Move your Air purifier and get rid of these pollutants in a matter of minutes.

Of course there are. Take a look through our different ranges of Air Purifiers, all with a different applicable room area.

How do our Air Purifiers provide these benefits?

Daikin unique's Catch & Clean approach 3 steps to decompose harmful substances

Get support, guides & logins

Contact Us

Get information & support

Contact a Daikin installer

Contact Us

Get installer information & support

Contact Us

Get information, CPD and certifications

Contact a Daikin installer

Contact Us