Heat pumps and radiators - the perfect pairing?
How to combine radiators and heat pumps for efficient home heating
Want to enjoy efficient, low-carbon home heating without replacing all your radiators? Modern air source heat pumps can work with most existing radiators, delivering cost savings and lower emissions. Success depends on radiator type, flow temperature, system design, and correct sizing. Upgrading to low-temperature or aluminum radiators boosts efficiency and comfort. In this guide, you’ll learn how heat pumps and radiators can work together, which radiator types perform best, what installation considerations matter, and how to plan a cost-effective, high-performance system.
Can heat pumps work with radiators?
Yes, heat pumps can work with radiators. It’s a common misconception that heat pumps require underfloor heating and simply cannot work with radiators designed for boilers. In fact, most new and existing radiator installations can work efficiently when paired with an air source heat pump system. Many domestic radiators are compatible with heat pumps, so you don’t always need a completely new emitter system.
The rising popularity of air source heat pumps for home renovations and new builds is driven by efforts to decarbonise heating and reduce running costs. For example, certain heat pump models can deliver flow temperatures up to 75 °C or more, allowing them to work with radiators originally sized for boilers.
While heat pumps can work with radiators, key factors such as radiator size, flow temperature, and system design must be considered to ensure optimal performance.
How do heat pumps work?
An air source heat pump extracts heat from the outside air and transfers it into your home’s heating circuit. The process is similarly to a refrigerator in reverse: the outdoor unit draws in outside air, the refrigerant evaporates, is compressed to raise its temperature, and the heat is then transferred to water circulating inside the home.
Compared with ground-source systems, which draw heat from the ground or groundwater, air source systems typically cost less to install and require less intrusive ground works, but may have slightly lower efficiency in extremely cold conditions.
In a typical heat pump cycle: ambient air or ground → refrigerant coil → compressor (raises temperature) → condenser → heat exchanger → warm water circulating to emitters.
The warm water is then pumped through radiators or other heat emitters, releasing the heat into the rooms.
Understanding water leaving temperature in heat pumps
The term “water leaving temperature” (also called “flow temperature”) refers to the temperature of the water as it leaves the heat pump unit and enters the heating circuit - whether radiators or underfloor heating. This parameter is significant because the heat output of the emitters depends directly on how hot that water is. For example, traditional high-temperature radiators are designed for flow temperatures of around 70–75 °C.
High temperature heat pumps can deliver water up to approximately 75°C, even at external temperatures down to –10 °C. This capability allows them to work with conventional radiators in many cases.
This ability to reach up to 75°C makes modern high-temperature heat pumps compatible with most radiator systems, including older ones. Older radiators were originally designed for higher water temperatures, so being able to supply similar heat levels ensures that these systems can still deliver comfortable indoor heating without needing a full radiator replacement. This makes upgrading to a heat pump both practical and cost-effective for existing homes.
High water temperatures vs efficiency: the trade-off
There is a trade-off in heat pump systems between leaving water temperature and system efficiency, typically measured by the Seasonal Coefficient of Performance (SCOP). The higher the required temperature of the water (for example to match a radiator sized for high temperature), the harder the heat pump must work and the lower the efficiency becomes. This is reflected in a reduced SCOP as the water leaving temperature increases.
When radiators are sized for low-temperature operation and the flow is kept lower, the system achieves better performance. For example, if a heat pump must deliver water at 70 °C rather than 45 °C, more electricity is needed per unit of heat, reducing SCOP and increasing running cost.
For this reason, low-temperature heating systems, such as underfloor heating or oversized radiators, are recommended. These systems allow the heat pump to operate more efficiently, maintain lower water temperatures, and keep energy costs lower.
Radiator types and performance
Home-heating radiators connected to a water circuit come in a variety of types, and understanding their differences helps you make informed decisions about your heating system:
- Panel radiators (flat steel panels): The most common type, featuring flat steel panels that efficiently emit heat and blend seamlessly with modern interiors. They perform well at low water temperatures
- Towel radiators: Typically found in bathrooms, they provide warmth while offering a convenient place to dry towels.
- Aluminum radiators (lightweight, high-conductivity): Lightweight with excellent heat conductivity, these radiators warm up and cool down quickly, offering better temperature control and energy efficiency.
- Cast iron radiators: High temperature radiators often found in older or historic homes.
Each type has unique performance characteristics. The heat output of a radiator is determined by its surface area, the temperature difference between the radiator surface and room air, and the flow temperature of supplied water.
For a given flow temperature, a radiator with a larger surface area or higher thermal conductivity delivers more heat. When operating at lower flow temperatures (as is typical with heat pumps), radiators may need to be larger or made of more conductive materials to deliver the required output.
Aluminum radiators: ideal partners for heat pumps
Aluminum radiators are particularly well suited to low-temperature heat pump systems. Aluminum has very high thermal conductivity compared with steel or cast iron, allowing faster uptake of heat and quicker warm-up times. For example, aluminum radiators use less water and reach temperature quicker, meaning less energy wasted.
In addition, they are lighter, easier to install (especially on walls that cannot support heavy radiators) and often have modern styling, making them appealing for renovations. Because heat pumps operate more efficiently at lower water temperatures, a radiator that heats up quickly and emits effectively at lower temperatures can significantly improve overall system performance.
In practice, if a household replaces a steel radiator sized for 70 °C flow with a properly sized aluminum unit, they may avoid the need to install underfloor heating or oversized new radiators.
Do you need to replace existing radiators?
You don’t necessarily need to replace existing radiators when installing a heat pump. It depends on the existing emitter's size, age, placement and the overall heat loss of the home.
A simple rule of thumb is to assess condition, heat delivery and placement.
First, check the condition of your radiators. Visible rust, corrosion, leaks, or frequent repair needs usually indicate internal wear that reduces efficiency and reliability. In these cases, replacement is often the better long-term option.
Next, consider how evenly and quickly they heat the room. Radiators that warm up slowly, have persistent cold spots even after bleeding, or struggle to keep a room comfortable are often no longer performing efficiently. In those cases, upgrading can improve comfort and energy performance.
Finally, assess size and placement. Larger, modern radiators that are fully exposed and not blocked by furniture or curtains tend to perform better, especially at the lower water temperatures used by heat pumps. Smaller or older radiators that need to run very hot to heat a room may be undersized for efficient heat pump operation.
Ultimately, a room-by-room heat-loss assessment carried out by a qualified installer is essential. This ensures radiator output is properly matched to the heat pump system and confirms whether the existing setup is sufficient or if upgrades are advisable.
Upgrading to low-temperature radiators
Upgrading to low-temperature radiators is a beneficial move when installing a heat pump system. These emitters are designed to operate efficiently at supply water temperatures of 35-55 °C. For house-owners this means: improved compatibility, longer lifespan for the heat pump (because it doesn’t have to run at high temperature), and better overall performance.
Radiators for heat pump systems may need about 2.5 times the surface area of a typical radiator sized for a boiler system in order to maintain comfortable temperatures at the lower supply flow.
Common materials for low-temperature models include aluminum and steel panel radiators designed for larger surface areas, but these typically cost more per unit. However, the upfront cost is offset over time by better efficiency and lower running costs than forcing an older radiator to work at higher flow.
Air source heat pumps and radiators in older homes
One common concern is whether an air source heat pump will work in older, less insulated homes, especially when using radiators. The answer: yes, and they’re ideally installed during a renovation, but you must factor in potentially higher heat loss and assess radiator capability.
For example, if existing radiators have large surface area and the home has decent insulation, they may be adequate for a heat pump. But in many older homes with high heat loss (solid walls, poor insulation, draughts), it might be necessary to install larger radiators or additional emitters to meet the heating demand. There is no need to replace all emitters. A radiator system that was marginal for a gas boiler may be insufficient for the gentler flow of a heat-pump system unless upgraded.
The role of sizing: heat pump and radiator matching
Correct sizing of both the heat pump unit and radiator emitters is critical. If the heat pump is undersized relative to the home’s heat loss, you’ll suffer poor comfort and possibly freeze-risk.
If the heat pump is oversized, efficiency drops and upfront costs increase unnecessarily. Likewise, if radiators are undersized for the required flow temperatures and heat demand, rooms will take longer to warm up or may never reach the desired temperature.
Radiator sizing for heat pumps typically assumes a lower ΔT (temperature difference between water and room air), which means larger heat emitters are required to deliver the same output. For this reason, a full room-by-room heat loss calculation carried out by a qualified installer is essential. This should be followed by correct radiator sizing and then selecting the appropriate heat pump output to match the property’s heating demand.
Installing a heat pump system with radiators
In a typical retrofit, installing an air source heat pump with existing radiators involves several key steps:
- Removal or adaptation of the existing boiler
- Installation of an outdoor unit and indoor modules
- Checking and, if necessary, replacing pipework
- Assessing and potentially upgrading radiators
- Re-balancing the heating system and installing controls (thermostats and TRVs)
- Setting the correct flow temperature and commissioning the system
Additional components such as radiator valves, pipework insulation, and buffer tanks may also be required. Modern high flow-temperature models (up to 70 °C) can make retrofitting to existing radiators simpler and reduce the need for major emitter upgrades.
Disruption is generally moderate. Some pipework may need adjusting and some radiators may need replacement to ensure compatibility with lower-temperature operation. Homeowners should discuss the schedule and expectations with the installer, including any need to bleed radiators, flush systems and ensure valves are appropriate for lower-temperature operation.
By setting realistic expectations and planning carefully, installing a heat pump system with radiators becomes a manageable upgrade rather than an overwhelming project.
What is a hybrid system and when is it useful?
A hybrid heating system combines an air source heat pump with an existing gas or oil boiler or another heat source to help cover peak demand or provide higher flow temperatures when needed.
In practice, this means that during very cold external conditions where heat pump efficiency naturally drops, the boiler automatically steps in. It provides higher-temperature water to the radiators, ensuring comfort even in the depths of winter.
Hybrid systems are sometimes used in older homes with high heat loss or radiators originally designed for high-temperature boiler systems. They can offer a transitional solution where insulation levels, emitter sizing, or budget constraints make a full heat pump conversion more complex.
However, when a property has been properly assessed and the heat pump and radiators are correctly sized and matched, a standalone heat pump system is typically sufficient without the need for a boiler backup. With accurate heat-loss calculations, appropriate radiator upgrades, and modern high-flow-temperature heat pumps where required, most homes can operate efficiently on a fully electric system.
Heat output considerations: calculating what you need
Radiator sizing is calculated based on room volume (or more precisely: heat loss), insulation levels, window area, and the required temperature difference between inside and outside. It is expressed in kilowatts (kW) or watts, which indicate the heating output needed to keep the space comfortable.
The required heating capacity is usually expressed in kilowatts (kW), with 1 kW roughly equivalent to 1,000 watts of heating power. This figure represents the amount of heat required to offset heat loss and maintain the desired indoor temperature.
Online radiator sizing calculators can provide a quick estimate, but for accurate results, especially in larger or older homes, it’s best to consult a qualified installer who can assess your property’s specific heating requirements, accounting for variables that online calculators simply cannot capture.
Sizing is particularly important when transitioning to a heat pump system, where getting the dimensions right makes all the difference.
Towel radiators with heat pumps
In bathrooms, towel radiators (heated towel rails) provide both heat and a place to warm towels. When used with a heat pump system, however, care must be taken as towel radiators typically have a smaller surface area and may require higher flow temperatures to deliver the same heat as a larger panel radiator.
Lower surface-temperature models can offer safety benefits, particularly in households with children, as they reduce the risk of burns from accidental contact.
As heat pumps favour lower temperatures, correct sizing becomes crucial. If a towel radiator is undersized for the lower flow temperature, it may take longer to warm up and deliver comfort. Therefore, when pairing a towel radiator with a heat pump, specify a model designed for low-temperature operation or size it up accordingly.
Avoid assuming that a towel radiator that worked well with a high-temperature boiler will automatically perform the same with a heat pump.
Electric radiators vs heat pump radiators
Electric radiators have their place as supplementary heating. However, for whole-home systems, water-based radiators paired with a heat pump usually deliver better efficiency, improved comfort, and lower running costs.
Electric radiators are best viewed as secondary rather than primary heating. When comparing running costs, a properly sized and installed heat pump operating at lower flow temperatures will typically outperform direct electric heating by a significant margin.
Panel radiators: traditional but adaptable
Panel radiators are the classic steel-panel types found in many homes. Although they were originally designed for higher flow temperatures (often ~70-75 °C) with a boiler, they can be made compatible with a heat pump system if sized appropriately for the lower supply temperature. The compatibility depends on whether they can provide required heat output at the lower flow.
For budget-conscious upgrades, retaining panel radiators (when correctly sized) can be a cost-effective route, rather than wholesale replacement. But some modification, or increased pipework and surface area, may be required to ensure performance with a heat pump system.
System design: zoning and smart control
In a heat-pump-to-radiator system, zoning (i.e., dividing the home into multiple heating zones with independent controls) and smart controls are particularly valuable. For example, separate thermostats and TRVs (thermostatic radiator valves) can manage bedrooms, living rooms, and bathrooms individually.
Smart thermostats and programmable heating schedules avoid unnecessary heating of unoccupied zones, thereby reducing waste and improving comfort. Proper zoning also means the heat pump can better match the actual demand, improving efficiency and reducing cycling.
Maintenance tips for heat pump and radiator systems
Maintenance for a heat pump and radiator system is similar to other hydronic systems but requires some extra attention due to lower flow temperatures and system specifics.
Regularly bleed radiators to remove trapped air, which can reduce output and cause cold spots. Associated pumps should be cleaned annually, and system pressure should be checked.
It’s wise to have an annual service by a qualified installer to check refrigerant levels, heat pump performance (SCOP), compressor and defrost cycle (for air source units). Check for unexpected noise or inefficiencies (e.g., radiators taking a long time to warm up) which may indicate issues such as dirty heat-exchanger fins, blocked airflow or insufficient radiator size.
Are radiators connected to heat pumps noisy?
Modern air source heat pumps and radiator emitters are designed for quiet operation. While the outdoor unit of a heat pump may emit fan noise, the radiators connected to a heat pump are almost silent.
Some indoor units operate at sound levels as low as 43 dB, which is quieter than normal conversation. The radiator system itself generates no noise.
Proper pipework insulation and anti-vibration mounting of the outdoor unit can further reduce perceived noise, especially in retrofit installations where routing may be more complex.
Heat pumps vs boilers: radiator performance comparison
When comparing heat pump systems with conventional boilers in the context of radiator performance, several differences emerge.
Gas boilers usually supply water at 70-75°C and are not designed for low-temperature operation. Heat pumps, by contrast, can operate across a range of 45–75 °C, allowing you to lower flow temperatures and reduce energy consumption. However, this depends on the radiators connected to the system. If existing radiators are kept, they will probably operate at high temperatures. For replaced or new radiators, a lower temperature will be possible.
From a sustainability perspective, heat pumps deliver substantially lower carbon emissions and, when properly designed, can reduce running costs significantly. Boilers offer faster response times and higher flow temperatures, but they burn fossil fuel with an associated higher carbon footprint.
Air source heat pumps: leading the low-carbon transition
Air source heat pumps are a key technology in the move to low-carbon home heating. Since they operate by transferring ambient heat rather than burning fuel, they can reduce CO₂ emissions significantly compared to gas or oil boilers.
The compatibility with radiators, when done correctly, means that many homes don’t need to move to underfloor heating to decarbonise their heating system. Heat pumps are suitable for both new-build and modernisation projects, even with conventional radiators.
In addition, with rising policy and incentives in Europe for heat pump installations, choosing a system now can help future-proof a home, align with regulatory targets and potentially unlock grant funding.
Common mistakes to avoid
When pairing heat pumps with radiators, several common mistakes can reduce performance and efficiency:
- Installing a heat pump without taking into account the required water temperature for the heat pump. Systems must be selected to handle the temperature range needed—up to 75 °C if connecting to existing radiators.
- Using radiators sized for high-flow gas boilers without adjustment. Best practice often requires radiators around 2.5 times larger than a standard boiler system to achieve equivalent output at lower flow temperatures.
- Overlooking the need for higher surface-area emitters for low-temperature operation.
- Neglecting pipework or insulation upgrades. While not always required, skipping these can significantly impact performance. Saving a few hundred euros on installation might cost thousands in inefficiency over the system's lifetime.
Plan carefully, size correctly, and don't cut corners. Doing it properly ensures better comfort, higher efficiency, and lower running costs.
Accessories that enhance performance
Several accessories can notably enhance your heat pump and radiator system's performance.
While not strictly essential, each offers clear benefits:
- Thermostatic radiator valves (TRVs) or smart radiator valves enable zoning and individual room control
- Flow meters can be useful to track system performance
- Aluminum or anti-corrosive internals in radiators reduce risk of galvanic corrosion when mixing metals
- Noise-reducing mounting brackets or decouplers can reduce vibration from circulation pumps or the outdoor heat pump unit
Using these accessories helps optimise system performance, reduce running costs, and increase comfort.
What ultimately determines success with heat pumps and radiators
With careful planning and expert consultation, a heat-pump-plus-radiators system is a smart and sustainable path to comfortable home heating for today and tomorrow. What's needed is thoughtful implementation, getting the details right so that heat pumps and radiators can work together to become an effective partnership.
Key takeaways
Success depends on flow-temperature design, radiator sizing, and heat-loss calculation
Evaluate and, if needed, upgrade radiators and controls to improve efficiency
Choose an installer experienced with low-temperature heat pump systems
Consider aluminum or low-temperature radiators for optimal performance and faster heat-up
Plan the system layout and zoning to maximise comfort and minimise energy waste