Skip to main content

Find out in this blog

A heat pump is a very efficient low-carbon technology. It uses renewable energy sources to provide heating, hot water and cooling for your home. This energy is released through connected emitters such as radiators, underfloor heating, heat pump convectors and your hot water system.

In this article, we look at heat pump connections and how they combine to create the optimum temperature for your home.

A heat pump can connect to heat emitters just like a traditional fossil fuel boiler does. The difference is in how it generates heat, rather than how it distributes it.

Instead of burning fossil fuel to create heat, a heat pump absorbs heat from renewable sources – air, ground or water – and uses a process of evaporating and condensing refrigerant. The result is a more efficient, cleaner form of heating.

Combining a heat pump with radiators

There are two types of radiators: high- and low-temperature.

High-temperature radiators tend to be found in older properties. The water inside them is heated to between 60 and 70°C.

You can use a high-temperature radiator with a high-temperature heat pump or a hybrid heat pump, which combines a heat pump and a gas-condensing boiler. This hybrid solution automatically boosts your system as required to maximise efficiency while reaching higher temperatures.

Today, there are many high- and mid-temperature heat pumps that deliver a flow temperature above 60°C. These are ideal for connecting to an existing piping system and older heating systems. Heat pumps also work perfectly with low-temperature radiators, which are usually found in newer houses. In both cases, the heated refrigerant circulates through a heat exchanger, which transfers the heat to water. This then circulates through pipes to the radiators.

Heat pumps with underfloor heating

A heat pump combined with hydronic, or water-based, underfloor heating can be a great way to heat a home. Heat pumps are most efficient at lower temperatures, and underfloor heating works at much lower temperatures than radiators. Underfloor heating is also energy-efficient and comfortable.

Hydronic underfloor heating is particularly compatible with a heat pump. It requires minimum energy and can be powered mostly from renewable sources.

Heat pump convectors

Another option is a heat pump convector (HPC), also known as a fan coil unit. It’s similar to a radiator, in that both use convection to heat a room, but the process is much faster because there’s a small fan behind it to speed up the heating cycle. So it can create the same room temperature as a traditional radiator with lower water temperatures inside, offering energy savings.

A heat pump convector is compatible with underfloor piping and radiators in a multi-zoning installation, or it can replace outdated radiators when combined with low-temperature heat pumps. It gives you higher capacities from a low-temperature heat pump for maximum efficiency.

Choosing the right heat pump connection

Ultimately, choosing the best emitters to combine with your heat pump will depend on your property, budget and needs. Whatever your requirements, there is an emitter for you.

We always recommend discussing the options with your installer, including the right emitters. That way you can be sure you have the right solution for your home.