Skip to main content

Find the best heating system for your home: know the options when replacing your heating system

Are you replacing an existing heating system or considering a new one? Then you might be thinking about moving away from fossil fuel systems towards something less affected by rising energy prices and with a lower impact on the environment.

Heating system options

Every home has different needs. Choosing the right heating system depends on the sort of home you live in, your budget and your lifestyle. There are many alternatives, depending on what you’re looking for.

Let’s consider the options that have a low environmental impact.

Air-to-water and ground-source heat pumps

Heat pumps come in various types: air-to-water, high-, mid- or low temperature, or ground-source.

They use up to 75 % renewable energy from the air or ground and connect to emitters to provide you with heating, cooling and hot water. Heat pumps are a complete home solution, with different types to match any need. For example, high-temperature air-to-water heat pumps are ideal for older homes that use radiators.

Hybrid heat pumps

Hybrid heat pumps combine existing gas or oil boilers with heat pump technology, switching automatically between the two to provide the most efficient performance.

You can combine them with a range of emitters to provide heating, cooling and hot water. They’re a great option for boiler replacements and a cheaper alternative to other heat pumps.

Air-to-air heat pumps

Air-to-air heat pumps, also known as air conditioners, offer an efficient heating, cooling and air purification solution. Easy to install and cost-effective, they work in any kind of home, old or new, detached, terraced or apartment.

They also offer several options, with single or multi-split solutions meaning you can connect up to five indoor units to one outdoor unit. There’s even an option to connect to a domestic hot water tank.

What’s next when replacing your heating system?

Whether you want to get rid of fossil fuels or take the first steps to reducing your dependence, there are several factors to consider. Think about cost, sustainability, durability and efficiency. Finding the best solution to replace your system might seem daunting, so talk to one of our experts or an installer about the options.

To learn more, read our blog on why investing in a heat pump is a smart move. And if you’re still not sure switching is a good idea, read our blog on heat pumps vs gas boiler systems.