Skip to main content

Considering replacing your fossil fuel heating system with a heat pump? We weigh up the advantages of heat pumps and gas boilers.

Rising energy prices and the need to protect the environment are causing many people to think more about their household energy use. Heat pumps are increasingly being seen as the best alternative to fossil fuel systems. Let's explore the pros and cons of the two.

A heat pump is a very efficient low-carbon technology. It uses renewable energy sources to provide heating, hot water and cooling for your home.

It extracts heat from the air, ground or water, making it very cost-effective to run. A gas boiler, on the other hand, is a fossil fuel-based system that produces carbon emissions.

Heat pump vs boiler costs

One of the main advantages of a gas boiler is the installation cost: the initial investment of a gas boiler is cheaper than that of a heat pump.

However, in the long term, a heat pump proves to be cheaper on running costs. It takes most of its energy from renewable sources and requires only a small amount of electricity to power it. So it cuts your energy bills.

Depending on the type of heat pump you choose, the initial purchase and installation cost could vary. A hybrid heat pump, for example, still uses a gas connection but also runs on electricity and renewable energy. It can therefore represent a more affordable way to start using renewable energy.

Another way to cut costs is to check for funding incentives to encourage homeowners to switch to renewable energy.

Environmental impact of heat pumps and fossil fuel systems

Heat pumps offer a very sustainable and efficient alternative to fossil fuel systems. As the world strives towards net zero carbon, we will see a push towards this form of renewable energy.

Heat pumps mostly use renewable energy (around 75%); for the rest it runs on electricity. Air-to-water heat pumps use heat from the air, while ground source heat pumps use heat from the ground.

This means they are far superior to fossil fuel systems when it comes to environmental impact. Gas or oil boilers produce emissions that are harmful to the planet.

The flexibility of your heating system

Another consideration is flexibility. Fossil fuel systems are an established solution for radiators and hot water, but did you know heat pumps can also provide cooling?

The versatile nature of heat pumps means they can be connected to various emitters to provide an all-in-one system for your home.

You can optimise your choice of heat pump further by combining it with solar panels or thermal storage.

In conclusion

Heat pumps are an increasingly common alternative to fossil fuel systems, such as gas boilers. That's due to their many benefits: running cost, efficiency, flexibility and environmental impact.

There are various options to ensure the optimum system for your home, including a hybrid solution as an affordable entry to renewable energy.

The right system for you will depend on your budget, needs, home and lifestyle. Discuss the options with your installer and find out what works for you.