With the new Daikin Emura, Daikin brings together the best of design and technology to help you achieve your perfect indoor climate: Daikin Emura keeps you cool in summer, and warm in winter. The new air conditioning unit also surprises with its curved design – pure elegance!
“Daikin Emura blends harmoniously into your interior”
Daikin Emura includes a wall mounted indoor unit, remote control and outdoor unit. Beautiful and intelligent design that blends harmoniously into your interior: high-end yet affordable. Daikin Emura will even make your walls proud.
Remarkable design
With a width of only 90 cm, Daikin Emura is proud to be different. Thanks to its curved panels, the indoor unit has a unique 3D shape. The curved lines refer to the harmonised airflow, but also create a visual effect in your interior: they create shadows and make Daikin Emura really come to life.
“A wall mounted air conditioning unit always has a visual impact. I believe it can also be a design statement. Using shadows is the most natural way to make product and interior design much more interesting”, reveals Hiroyasu Kosuge, Daikin Emura brand designer.
The remote control has the same sleek design and fits your hand perfectly. Both the indoor unit and the remote control are available in silver, matt white and matt black. The redesigned outdoor unit comes in ivory white.
Optimised air distribution
It goes without saying that a room only needs to be cooled or heated when you’re actually in it. Daikin Emura uses an intelligent thermal sensor and specially designed flaps to (re)direct the airflow and ensure a constant and harmonised temperature throughout the room. Thanks to the new heat boost function, Daikin Emura quickly heats a room when starting up, ensuring the set temperature is reached faster
Whisper quiet operation
A Daikin Emura air conditioner runs so quietly you’ll almost forget it’s there. A specially designed fan optimises the airflow for high performance levels at low sound levels, making Daikin Emura practically inaudible in operating mode.
Better indoor air quality
With built-in air purifying filters and Flash Streamer technology, Daikin Emura captures dust particles, breaks down allergens and removes bothersome odours, providing you with better, cleaner air. That’s how the Daikin Emura air conditioning unit keeps your home healthy.


User-friendly control
Control the indoor climate with ease. The new remote control introduces a simplified design with strong focus on the most important functionalities. You can easily access all other features via the self-explanatory menu or from anywhere at any time with the intuitive Onecta app on your smart devices.
Maximum efficiency
Whether it’s extremely hot or cold outside, you expect your air conditioner to perform all year long in the same stable way. Daikin Emura is engineered to perform every season and provide year-round comfort in the most energy-efficient way. Your guarantee for best-in-class performance with seasonal efficiency values up to A+++ in cooling and heating, resulting in a low environmental impact and low energy bill.

Two prestigious awards
The new Daikin Emura blends elegant design with state-of-the-art technology and outstanding efficiency. No wonder it was honoured with this year’s Red Dot Product Design Award and iF Design Award – two of the most prestigious design awards in the world that reward remarkable product innovation.

DAIKIN EMURA FTXJ-AW MATT WHITE

DAIKIN EMURA FTXJ-AS SILVER

DAIKIN EMURA FTXJ-AB MATT BLACK
About Daikin Europe
N.V. Daikin Europe N.V. is a major European producer of air conditioners, heat pumps and refrigeration equipment, with approximately 5,500 employees throughout Europe and 10 major manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Turkey and the UK. Globally, Daikin is renowned for its pioneering approach to product development and the unrivalled quality and versatility of its integrated solutions. With more than 90 years’ experience in the design and manufacture of heating and cooling technologies, Daikin is a market leader in heat pump technology.