Skip to main content

Daikin's new 'Commission with Confidence' service brings stability to R410a prices

13.07.18

In July 2018, Daikin Airconditioning UK Ltd launched two ground-breaking service packages that will guarantee the cost of R410A refrigerant. The packages are at a set fee until 31st March 2019, when purchased together with new VRV systems.

The ‘Commission With Confidence’ packages aim to bring stability and confidence to the market,  which has experienced turbulent price increases for refrigerant as a result of quota restrictions set by the 2015 European F-gas Regulation. 

Daikin is the only air conditioning manufacturer in the industry that also produces refrigerant gas (via Daikin Chemicals) and so is able to guarantee the supply of R410A refrigerant trim charge as part of a commissioning package for a set fee, giving Daikin customers ultimate confidence from tender to installation of a VRV system. 

Mark Dyer, Commercial Director of Daikin UK said, “The launch of Daikin’s Commission With Confidence service is an exciting move for our organisation and the industry as a whole. Our aim is to contribute to the stability of the HVAC market by helping to protect our customers’ businesses from soaring refrigerant prices. We hope this will give our customers confidence that they can commission VRV systems throughout 2018 and into 2019 without worrying about fluctuating installation costs.”

The Commission With Confidence packages are available to purchase now and current prices are guaranteed until 31st March 2019, including trim charge. Two packages are available.

  • Standard package includes R410A trim charge and on site commissioning support
  • Premium package includes R410A trim charge, commissioning support and cloud services.

There are three different price levels for each package, depending on the capacity of the system.

 Standard servicePremium service
VRV System SizeEx-VAT price (non-discountable) per systemEx-VAT price (non-discountable) per system
Size 4 to size 16 horsepower (inclusive)Set priceSet price
Size 18 to size 24 horsepower (inclusive)Set priceSet price
Size 26 horsepower and aboveSet priceSet price
Service includes  
Daikin service on site to assist with refrigerant systemYes Yes
All refrigerant required to cover trim charge for installationYes Yes
Initial cloud set upNoYes
Energy and system monitoring for 1 yearNoYes
1 annual monitoring reportNoYes

For more information on Daikin UK, visit www.daikin.co.uk and follow @DaikinUK on Twitter. 

For further press information, please contact Alicja Robertson or Giulia Kapp on 01932 879000, or email marketing@daikin.co.uk.  

 

Related articles