Skip to main content

Compact air purifier offers powerful lasting protection

Announcing the new MC30YB, the latest addition to join the Daikin family of air purifiers.

Designed to meet the needs of both residential and light commercial users, the MC30YB offers a cost-effective, low maintenance solution that creates a healthier indoor environment. Compact yet powerful, the MC30YB effectively and quietly reduces bacteria, viruses and other airborne contaminants, providing pure, healthy air to safeguard the health of household members, customers and employees.

Built-in performance and reliability for peace of mind

Housing advanced technology in a neat white space-saving tower cabinet, the MC30YB starts working immediately to deliver cleaner air. Airflow rates of 180 cubic metres per hour provide coverage of large surfaces up to 46 square metres (calculated according to NRCC 54013).

The combination of small dimensions (450 x 270 x 270 mm) and high output, together with its attractively low price and exceptionally long filter lifetime (10 years) make this latest air purifier ideal for use across a diverse range of locations from homes, retail outlets, banks and horeca applications to commercial offices, meeting rooms and healthcare settings.

One of the quietest units on the European market, with a dB(A) of 19 in quiet mode, the MC30YB is unobtrusive, working quietly in the background to maintain and improve air quality. An inbuilt SLEEP mode ensures a peaceful rest at night for householders.

Catch and clean

In common with other models in the Daikin air purifier collection, the MC30YB is equipped with an Electrostatic (HEPA) filter and Flash Streamer technology to ensure the cleanest air possible.

This unique approach captures and removes pollutants and allergens in 3 easy steps, offering clear benefits and demonstrable results.

 

Stage 1: Attraction - The MC30YB draws in air from a wide area in three directions to ensure comprehensive coverage.

Stage 2: Capture – the high-performance electrostatic HEPA filter traps up to 99% of particles between 0.1 µm and 2.5 µm. The electrostatic component collects dust more efficiently without clogging and with no pressure loss.

Stage 3: Decomposition – Daikin’s unique Streamer technology uses plasma discharge to eliminate harmful and dangerous substances caught on the filter through oxidation.

An integral deodorising filter absorbs and removes odour, while an inlet at the bottom of the front panel collects harmful substances at floor level. There is no need to replace the deodorisng filter during the unit’s lifetime and the electrostatic filter lasts for up to ten years, making the MC30YB an attractive lifecycle option.

 

Working together to create a cleaner environment

Jonas Bosman of Daikin explains: “At Daikin, ensuring the purity of air we breathe in indoor environments is a key concern. Our mission is to deliver safe, healthy and comfortable spaces, while minimising environmental footprint through the application of innovative technologies, working towards achieving Net Zero CO2 emissions by 2050.”

He concludes: “The MC30YB is an exciting addition to the Daikin air purifier range which will strengthen our offering as a leader in the market, while helping to protect individual health and well-being.”

The MC3OYB is now available. For more information visit: https://www.daikin.co.uk/en_GB/products/MC30YB.html

About Daikin

Air is essential to our existence. It has always been Daikin’s mission to make the air we breathe and live in the best possible. Our innovative products and solutions are designed to improve people’s health and well-being and reduce the environmental impact of heating and cooling. By 2050 Daikin aims to be carbon neutral throughout the full value chain and the full life cycle of its products and solutions.

Daikin Europe N.V.

Daikin Europe N.V. is a major European producer of air purifiers, air conditioners, heat pumps and refrigeration equipment, with 10,000 people employed throughout Europe and fourteen major manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Turkey, Austria and the UK.

Globally, Daikin is renowned for its pioneering approach to product development and the unrivalled quality and versatility of its integrated solutions. With more than 90 years’ experience in the design and manufacture of heating and cooling technologies, Daikin is a market leader in heat pump technology. Daikin VRV and Daikin Altherma are the most sold heat pump systems in Europe, with over 500,000 systems delivered to date.

Daikin Industries Ltd.

Daikin Industries Ltd. based in Osaka, Japan, employs around 89,000 people worldwide and achieved sales of € 23.7 billion in financial year 2021 (1 April 21 – 31 March 22). The company is the global market leader for heat pump and air conditioning systems, as well as air filtration. Daikin Industries Ltd. is the only air conditioning manufacturer in the world that develops and produces all important components such as refrigerants, compressors and electronics in-house.

Read more on www.daikin.eu and www.daikin.com

Get support, guides & logins

Contact Us

Get information & support

Contact a Daikin installer

Contact Us

Get installer information & support

Contact Us

Get information, CPD and certifications

Contact a Daikin installer

Contact Us