Skip to main content

How can I synchronize the BRC1H Auto operation mode between the Daikin Residential Controller app and a Sky Air unit?

For BRC1H

In order to synchronize the Auto operation mode between the Daikin Residential Controller app and the Sky Air wired remote controller, do the following:

  1. ​Install and connect the BRC1H remote controller to the Sky Air indoor unit. For installations using BRC1E, see the "How can I synchronize the BRC1E Auto operation mode between the Daikin Residential Controller app and a Sky Air unit?" FAQ item.
  2. Set the setpoint logic to "Indoor unit" in the Madoka Assistant app.

Changing the setpoint logic using the Madoka Assistant app

1. Open the latest version of the Madoka Assistant app.
2. Enable Advanced Settings:
        1. Go to the main menu.
        2. Select "About". Note that starting from Madoka Assistant version 1.10, "Advanced Settings" will be available under "App Settings" instead of under "About".

Madoka assistant app main menu

3. Select "Advanced Settings".

Madoka Assistant App About Screen

4. Toggle on the "Advanced Settings". A warning message appears.

Madoka Assistant App Warning Advanced Settings Window

5. Press "I understand". Advanced Mode is now enabled.

3. Go to "Unit settings".

Madoka Assistant App Unit Settings Window

4. Select "Setpoint logic".

Madoka Assistant App Setpoint Logic Window

5. Select the "indoor unit" option and press "Apply"​.

In order to synchronize the room temperature between the Daikin Residential Controller app and the Sky Air wired remote controller, configure the field settings for the wired remote controller either using the Madoka Assistant app or directly on the wired remote controller. See the steps below for more information.

Configuring the field settings using the Madoka Assistant app

1. Open the latest version of the Madoka Assistant app.
2. Enable Advanced Settings:
        1. Go to the main menu.
        2. Select "About". 

Madoka Assistant App Home Screen

3. Tap "Application version" 5 times to enable installer mode.

Madoka Assistant App About Screen

4. Set the installer mode to "Temporary".

Madoka Assistant App Installer Mode - Temporary

5. Return to home screen and select the remote controller.
6. Go to "Unit settings" from the settings menu.

Madoka Assistant App Unit Setting Screen

7. Go to "Field Settings".

Madoka Assistant App Field Settings Screen

8. Select item 02 under "Mode 10" and set the value to 02.

Madoka Assistant App Edit Field Screen - Mode 10, Value 02

9. Select item "01 Thermostat sensor" under "Mode 1c" and set the value to "01 - Indoor unit thermistor".

Madoka Assistant App Edit Field Screen - Mode 1c, Value 01

10. In the top right corner, tap "Apply". Confirm by tapping "Apply" again in the confirmation pop-up.

Madoka Assistant App Apply Setting Pop-Up

11. Select "Apply to remote controller".

Madoka Assistant App Apply Remote Controller

12. Verify that the remote controller is restarting. The new settings are applied once the remote controller has restarted.

Madoka Assistant App Restarting Controller

Configuring the field settings on the wired remote controller


Note that you do not have to configure the field settings on the wired remote controller if you have already configured them using the Madoka Assistant app (see above).

1. ​Press the middle button (circle) and keep it pressed until the information screen appears

Wired Remote Controller Middle Buton (Circle)

2. Press the left button (minus) and the middle button (circle) simultaneously and keep them pressed until you enter the installer menu.

Wired Remote Controller Left and Middle Button

3. Navigate to the field settings menu for the indoor unit. The menu icon shows a document with a wrench in front of it.

Wired Remote Controller Field Settings Document Wrench

4. Select Mode 10 and confirm your selection.

Wired Remote Controller Mode 10 Confirm

5. Change the setting (SW) to 02 and set the value to 02.

Wired Remote Controller SW To 02

6. Confirm your selection.

Wired Remote Controller SW To 02 Confirm

7. Select Mode 1c and confirm your selection.

Wired Remote Controller Mode 1c and Confirm

8. Change the setting (SW) to 01 and set the value to 01. Confirm your selection.

Wired Remote Controller SW To 01 Confirm

9. In the field settings menu, select "X" to return to the previous menu.

Wired Remote Controller Select X

10. In the installer menu, navigate to and select the arrow icon to restart the wired remote controller and apply the new settings.

Wired Remote Controller Arrow Icon to Restart