Skip to main content

Can I change the date and time of the unit’s user interface with the Daikin Residential Controller app?

When you add your first unit to your user account, the app will automatically try to update the date and time of the user interface if it differs more than 15 minutes with that of the mobile device. For some units, however, you need to change the date and time of the user interface manually, if required.

Network gateway: BRP069A6x (Daikin Altherma heat pump system)

Depends on the generation of the heat pump system:

2nd generation: to change the date and time of the unit's user interface, you have to do this manually on the user interface.

3rd generation:

  • MMI <= 5.2.0  : to change the date and time of the unit's user interface, you have to do this manually on the user interface
  • MMI  =  5.2.0  : the date and time can be automatically synchronised with that of your mobile device

Network gateway: DRGATEWAYAA (Daikin gas condensing boiler system)

The date and time can be automatically synchronised with that of your mobile device

When automatic synchronisation of date and time is possible, here is how you do it:

1.      In the home screen, press the gear icon

2.      Select “Date and time”

3.      Select “synchronise with mobile device date and time”

4.      Continue by confirming the pop-up.