Switch a broken boiler for a far more eco-friendly option
If you fear your central heating boiler won't make it through another winter, have you thought about replacing it with an eco friendly heat pump?
Using energy from the air, ground, water or solar panels, this is the low-carbon alternative to a traditional gas or oil boiler. But how a heat pump works and what benefits it might bring are a mystery to most of us. Only 27,000 heat pumps were installed in UK homes las year, compared with about 1.7 million gas boilers.
"There is still so much education to do about heat pumps, both for consumers and in the heating trade, but they are the future", says Iain Bevan, the commercial manager for heating and renewables at Daikin, a heat pump manufacturer.
Indeed, from 2025 developers will be obliged to fit air or ground-source heat pumps in new homes as part of the government's bid to cut emissions and make us all more energy efficient.
Heat pumps are included in the Government's new Green Homes Grant scheme, which allows owners to claim two thirds of the cost of energy-efficient measures up to £5,000 (a maximum of £10,000 is available for those on low incomes and in receipt of certain benefits). Homeowners make up any shortfall in costs themselves.
The Energy Saving Trust says you should expect to pay between £9,000 and £11,000 for an air-source heat pump, the most popular UK choice. That's more than three times the cost of a typical new gas boiler with thermostatic radiator valves, excluding radiators (£2,300).
However, with a heat pump, average savings on fuel bills may eventually recoup at least some of the cost in installation. Igloo, a challenger company, estimates £3,000 over seven years, typically.
First step - find a reputable installer
You must find an experienced and recommended installation company that can undertake a full assessment of your home's needs. This will account for radiators and underfloor heating, the number of occupants (for hot water use) and insulation. Underfloor heating and heat pumps are a good combination; it can eliminate the need to increase radiator size to ensure enough warmth goes into each room.
The installer must be a member of the Microgeneration Certification Scheme to comply with legal standards. The website has a useful postcode search function to help you find a local firm (mcscertified.com).
Alternatively, you can also rely on the expertise of a qualified installer from Daikin's Sustainable Home Network. They can advise you on how to make the switch to sustainable heating and install your new system. Visit the Daikin Installer Finder to learn more (Daikin Installer Finder).
What is a heat pump?
A heat pump is classed as "renewable" because it uses natual elements. An air-source heap pump extracts warmth from the air; it is a box that can be fixed to an exterior wall or roof, or stand alone. A ground-source heat pump requires generous outside space and is buried under the soil. A water-source heat pump takes water from your own lake, river or stream. There are also heat pumps that work in conjunction with photovoltaic solar panels. Checkatrade has a useful guide (bit.ly/3730qQw).
How does it work?
Think of a heat pump like a fridge in reverse, Bevan says. A fridge extracts heat from the interior so it feels cold inside. This heated air is released externally, which is why the coil on the back of your fridge feels warm. A heat pump worls the other way round, by extracting warmth from the outside air and releasing it into the hot water and central heating system.

Step 1
Air is blown across an evaporator, where heat enertgy from the air is absorbed by a refrigerant.
Step 2
The heat energy increases the refrigerant's temperature, and it evaporates from a liquid to a gas, storing the captured energy.
Step 3
The refrigerant passes into a condenser, where it cools and condenses back into a liquid, releasing the heat energy.
Step 4
The heat is transferred into the home's hot water circuit.
What are the benefits?
Cheaper energy bills. as well as lower carbon emissions, minimal maintenance and no danger of potentially hazardous gases, such as carbon monoxide, says Jessica Tan, the managing director of Ovo Smart Home. Radiators won't be searingly hot to the touch because heat pumps deliver heat at lower temperatures over longer periods; this could be good for young families.
And the drawbacks?
How quickly you make savings depends on the energy source you already use. The most dramatic results would be achieved by ditching a solid fuel or eletric-powered system, not gas. if you have a combination boiler you'll need a cistern tank to store your heated water. A cistern can go in the loft, utility room, cellar or basement (you don't need gravity to feed this kind of system). However, not every home will have the space. Bevan says that manufacturers are developing tanks to fit under a kitchen sink, or bolt on to the outside of a house.
A happy hybrid?
A hybrod heat pump, known as a bivalent system, could be a good idea if you live in a colder part of the UK but want to reduce your dependance on gas or oil. It is made up of two parts; an air-source heat pump that operates when the weather is milder and a boiler to kick in when the temperature drops. An automatic "weather compensation" programme manages the switch. typically when the temperature falls below 7C.
Think of the neighbours
They may not share your enthusiasm for renewable technologies, especially as heat pumps have a reputation for being noisy. Noise levels must be assessed to ensure the heat pump is not a nuisance. Look for a model with the Quiet Mark accreditation (quietmark.com).
Download the original article
Get a PDF copy of the original article from The Times newspaper.

Fund the switch to an energy-efficient heat pump? It's as easy as 1, 2, 3
With time-limited cashback, government grants and financial incentives available, there's never been a better time to make your change for good.