Skip to main content

Enjoy lower running costs and reliable comfort with efficient heat pump heating.

If your home uses heating oil, the winter routine may feel all too familiar. Checking the oil tank level, calling suppliers, comparing fluctuating prices, then waiting for the delivery truck to arrive.

Recent global events have made this routine more uncertain, with some households seeing the cost of filling their oil tanks rise sharply. Because heating oil is not regulated, prices can change quickly and without warning, making it difficult to plan ahead.

For many homeowners, this lack of control is becoming a key reason to consider alternatives.

Avoid unpredictable fuel prices

Heating oil prices can fluctuate significantly, leaving households exposed to sudden increases in costs. For homes that rely on oil, this can make budgeting for heating more challenging.

A heat pump offers a different approach. Running on electricity and using renewable energy from the air outside, it removes the need for fuel deliveries and reduces reliance on volatile oil pricing.

This shift can help bring greater stability to household energy costs over time.

Lower running costs over time

Heat pumps are designed to operate efficiently, typically delivering three to four units of heat for every unit of electricity used.

For a typical 4-bedroom home currently using oil, this level of efficiency can translate into running cost savings of over £1,200 per year, depending on the property and usage.

Over time, these savings can make a meaningful difference to overall household energy spend.

A practical long-term investment

While the upfront cost of a heat pump can be higher than replacing an existing boiler, lower running costs help to offset this over time.

Many homeowners find that the overall investment can be recovered in around five years, depending on factors such as property size, insulation and system design.

Beyond this point, the system continues to deliver ongoing savings, alongside improved comfort and more predictable costs.

Upfront costs are now lower

Government support has made heat pumps more accessible than in the past.

Through the Boiler Upgrade Scheme, homeowners in England and Wales can receive a £7,500 grant towards installing an air source heat pump. In Scotland, support can include a grant and an interest-free loan of up to £18,000.

With the current 0% VAT rate on heat pump installations, the overall cost can be comparable to replacing an ageing oil boiler and storage tank.

Efficient heating for modern homes

Heat pumps provide reliable heating and hot water throughout the year, even in colder conditions. Designed for continuous operation, they maintain consistent temperatures across the home.

Switching away from oil can also support carbon reduction. Heating oil produces around 2.5 kg of carbon per litre burned, along with other pollutants such as NOx, which contribute to poor air quality.

No tanks, deliveries or hidden risks

Oil heating systems come with practical challenges that many homeowners would prefer to avoid.

These can include:

  • Volatile oil prices that can change quickly and unpredictably
  • Oil deliveries that need to be scheduled and paid for in advance
  • Large storage tanks taking up space in the garden
  • The risk of oil theft in some rural areas
  • Potential costs and environmental impact if a tank leaks

A heat pump removes the need for stored fuel. There’s no oil tank, no deliveries and no risk of leaks from stored heating oil.

Improving your home’s appeal

Energy efficiency is becoming an important factor for homebuyers.

Research from Rightmove suggests that improving a home’s Energy Performance Certificate rating from an F to a C can increase property value by around 15%. Installing a heat pump can play an important role in improving a home’s EPC rating.

As more buyers look for energy-efficient homes with lower running costs, upgrading your heating system can make your property more attractive.

Find out more

With rising oil prices and increased awareness of energy efficiency, many homeowners are now considering alternatives to oil heating.

Case study: Moving from oil heating to a heat pump

“We moved into a bungalow with oil fired central heating just before Christmas. The seller was supposed to leave us with a quarter of a tank of fuel, but when we checked, it was nearly empty.

When we rang local suppliers, the cost of oil was extremely high, and there was no flexibility on price. If we wanted heating and hot water over Christmas, we simply had to pay. It was a frustrating experience.

That was the point we started looking for alternative ways to heat the property. As the bungalow was in an off gas area, an air source heat pump seemed like the right solution.

We’ve been really pleased with the result. The bungalow is warm, we have hot water when we need it, and our heating costs are far more predictable. Knowing we’ve also reduced our carbon footprint is the icing on the cake.
Homeowner, Clive Bull