Skip to main content

Make a smart investment: install a heat pump system when building a new house

As homeowners look to move away from fossil fuel heating systems, particularly in new builds, heat pumps are becoming an increasingly popular choice. They have a lower environmental impact and are more sustainable, as well as being more cost-effective. Here’s what you need to know if you’re considering one for your new build home.

Cost-effective and with a low environmental impact, heat pumps are an all-round heating, cooling and hot water solution. They transfer heat to emitters like radiators and underfloor heating, to ensure your home’s temperature suits your needs.

There are various types of heat pump, suitable for all types of home. These include air-to-air (often referred to as air conditioners), air-to-water and ground-source. In new build homes, the ideal heat pump is a low-temperature air-to-water heat pump.

What are air-to-water and ground-source heat pumps?

Air-to-water heat pumps use the external temperature to extract heat. These are the most common heat pumps, suitable for use in all types of houses: detached, terraced and apartments. A little electricity is required, though only around 25 % of the total energy used.

Ground-source heat pumps use a system embedded in the ground to extract heat. This makes them suitable for homes with the necessary land for a ground array or borehole system. Again, a little electricity is required.

For more information on the difference between air-to-water and ground-source heat pumps, see our blog.

What are the benefits of installing a heat pump in a new build home?

As a flexible heating, cooling and hot water solution, heat pumps are ideally suited to a new build home where you can choose which emitters to use, like underfloor heating, convectors or radiators. All your home needs are covered with one system.

A heat pump will also provide you with hot water. An indoor set-up that integrates a hot water tank is the standard format. You can combine heat pumps with additional heat sources, such as thermal stores and thermal solar panels, for hot water production. This gives you even greater efficiency. As heat pumps primarily use renewable energy, they can cut your energy bills, and installing a heat pump can increase the value of your home.

While they have minimal service needs, heat pumps do need proper maintenance to extend their lifespan.

Alongside all their other benefits, one of the biggest advantages of heat pumps is that they provide flexibility in shape, size and control. Opting for a heat pump ensures your home is energy efficient, sustainable and comfortable all year round.

Do you want to save energy with a heat pump for your new build home? Look no further than Daikin.