Skip to main content

Learn how installing a heat pump can improve EPC ratings and increase your property’s market value

Heat pumps not only enhance indoor comfort but also add significant value to a property. By improving a building’s Energy Performance Certificate (EPC) rating, reducing energy bills, and qualifying for government incentives, installing a heat pump can be a smart, future-proof investment for any British homeowner or developer looking to increase a property’s market appeal and resale value.

Installing a heat pump doesn’t just reduce your energy bills – it can increase the value of your home. In today’s market, energy efficiency is a key driver of property prices. Homes with lower carbon emissions and better EPC ratings command higher sale prices and generate stronger rental income. For homeowners looking to future-proof their property, a heat pump is one of the most effective upgrades you can make.

Boost your EPC rating. Boost your property’s value

Every property sold or rented in the UK must have an EPC – a legally required assessment of a building’s energy efficiency. A certified professional evaluates the property’s size, age, construction materials, insulation, and heating system to assign a rating from A (most efficient) to G (least efficient).

And this rating matters. Buyers and renters use EPC scores to judge long-term costs and sustainability, and will often pay more for homes with a better rating.

Heat pumps dramatically improve EPC scores. They are far more efficient than traditional gas or oil heating systems, and typically move a property up by one or more EPC bands. The size of the leap depends on two key factors:

  • The heating system being replaced (e.g. gas, oil, or electric resistance)
  • Whether radiators were upgraded or underfloor heating was installed alongside the heat pump

For example, a home previously rated E with a gas boiler could easily be upgraded to D or even C with a heat pump and radiator improvements.

What’s the value increase?

The impact on sale and rental value is tangible. A recent study by Knight Frank found that improving a home’s energy performance from band D to C added 3% to its value - around £9,000 on the average UK property. A two-band leap from E to C delivered an uplift of 8.8%, or more than £29,000.

Additional research from WWF and Scottish Power found that simply installing a heat pump added £5,000–£8,000 to the average home’s market value, excluding installation costs.

Mandatory energy standards reshape residential heating

In the UK, the Future Homes Standard (FHS) sets out that new homes will not be built with fossil fuel heating, such as a natural gas boiler. Considering the low penetration of district heating (heat networks currently meet approximately 2% of heat demand in the UK123), heat pump adoption is expected to increase in new homes under the FHS.

The introduction of the FHS will ensure that from 2025, an average home will produce at least 75% lower CO₂ emissions than one built to current energy efficiency requirements. The legislation will considerably improve the energy efficiency standards for new homes in the long run.

Incentives: subsidies help homeowners cut costs and carbon

With the Boiler Upgrade Scheme providing grants of £7,500 to pay for part of the installation, heat pumps are now within reach for thousands more homes. In Scotland, the Home Energy Scotland Grant and Loan provide funding for energy efficiency improvements and heat pumps In Scotland. It aims to support homeowners to make improvements and transition to renewable energy systems.

The bottom line

A heat pump isn’t just a heating solution – it’s a capital improvement. It enhances comfort, lowers operating costs, improves energy performance, and delivers a measurable return on investment when it comes time to sell.

If you’re planning to bring your property to market, or simply want to strengthen its long-term value, installing a heat pump could be one of the smartest moves you make.

More reasons to choose a heat pump