- Requirement
- Solution
- Kit List
- Result
After nearly two decades’ excellent service, failure of an air conditioning system based on the now-banned R22 refrigerant – making it impossible to replace failed components – left Coventry University Technology Park with no alternative but a total system replacement. The three storey Enterprise Centre is one of several buildings in the park, accommodating start-up and small technology businesses. When problems hit the air conditioning system, consultants Pick Everard and Daikin installer Envirotech Climate Control were called in. Technology Park manager Jane Rawlings-Purcell held several meetings with the Envirotech project team at the start of the project so that issues could be identified.
In a 12-week project, the centre’s entire air conditioning installation was replaced with a VRV IV heat recovery system from Daikin UK. Richard Cobb, an Associate at Pick Everard, says: “We designed and phased the works to limit disruption for occupants: all work within the building was conducted out of hours.” Envirotech Climate Control director Brett McKay says the centre now has nine condensing units in a compound behind the building. “There are three systems – one for each floor – giving a total of 136hp. Indoors, there are medium static pressure ducted fan coil units. Daikin heat reclaim VAM units provide energy efficient ventilation."
VRV IV heat recovery condesing unit
Medium static pressure ducted fan coil unit
Wired remote controller
Heat reclaim ventilation unit
iTouch Manager
Bacnet gateway interface
To give tenants some flexibility with office temperatures, fan coils and the ventilation units are individually controlled via Daikin wired remote controllers. Overall, the systems are controlled with a Daikin i-Touch Manager with a Bacnet gateway interface to link with a building management system. Jane Rawlings-Purcell says: “My expectations were exceeded and the result was a well-designed system, seamlessly installed without any hitches. It made a pleasant change to work with a very professional team that listened to our needs and managed the job faultlessly.” The Enterprise Centre installation has sparked a rolling project to replace R22 systems elsewhere in the park.